This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc26x2 TOF+AOA



我尝试使用SDK3.40运行ToF演示(AoA与ToF同时运行)。我将BOOSTXL-AoA放置在Passive上,Master使用固有的天线。Slave作为目标设备。在单独运行AoA功能时一切正常,但是我启用ToF功能后一直报错如下提示:

=== ERROR: Timeout reached while waiting for : Passive nodes to end TOF calibration ===

下面是我在Python文件下的设置,


同样,我在对应版本的UI界面可视化运行时,TOF结果也不能正常显示一直报错,而AoA功能一切正常。

所以,我想询问下尊敬的工作人员,这个问题是我哪里设置存在问题还是说该SDK版本存在这样的Bug或者是Passive端不应该外附BOOSTXL-AoA开发板。

附件里有对应的Python例程的日志,请注意查收

[2021-03-26 15:22:56,813] root -     INFO - Setting nodes : 
[2021-03-26 15:22:56,814] root -     INFO - Message receiver started
[2021-03-26 15:22:56,815] root -     INFO - RTLS Manager started
[2021-03-26 15:22:58,816] root -     INFO - Done setting node
[2021-03-26 15:22:58,889] root -  WARNING - ConstError('parsing expected 254 but parsed 0')
[2021-03-26 15:22:58,891] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_RESET_DEVICE", "payload": {"raw_payload": ""}}
[2021-03-26 15:22:58,895] root -  WARNING - ConstError('parsing expected 254 but parsed 0')
[2021-03-26 15:22:58,949] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_RESET_DEVICE", "payload": {"raw_payload": ""}}
[2021-03-26 15:22:59,102] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:22:59,153] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"eventType": 19, "addrType": 0, "addr": "80:6F:B0:EE:AD:32", "rssi": -63, "dataLen": 14, "data": "0A:08:52:54:4C:53:53:6C:61:76:65:02:01:06"}}
[2021-03-26 15:23:01,072] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN_STOP", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:01,224] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:01,225] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"eventType": 19, "addrType": 0, "addr": "80:6F:B0:EE:AD:32", "rssi": -62, "dataLen": 14, "data": "0A:08:52:54:4C:53:53:6C:61:76:65:02:01:06"}}
[2021-03-26 15:23:03,198] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN_STOP", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:03,302] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:03,303] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"eventType": 19, "addrType": 0, "addr": "80:6F:B0:EE:AD:32", "rssi": -61, "dataLen": 14, "data": "0A:08:52:54:4C:53:53:6C:61:76:65:02:01:06"}}
[2021-03-26 15:23:05,273] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN_STOP", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:05,425] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:05,425] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"eventType": 19, "addrType": 0, "addr": "80:6F:B0:EE:AD:32", "rssi": -62, "dataLen": 14, "data": "0A:08:52:54:4C:53:53:6C:61:76:65:02:01:06"}}
[2021-03-26 15:23:07,394] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN_STOP", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:07,550] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:07,550] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"eventType": 19, "addrType": 0, "addr": "80:6F:B0:EE:AD:32", "rssi": -62, "dataLen": 14, "data": "0A:08:52:54:4C:53:53:6C:61:76:65:02:01:06"}}
[2021-03-26 15:23:09,518] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN_STOP", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:09,672] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:09,672] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"eventType": 19, "addrType": 0, "addr": "80:6F:B0:EE:AD:32", "rssi": -61, "dataLen": 14, "data": "0A:08:52:54:4C:53:53:6C:61:76:65:02:01:06"}}
[2021-03-26 15:23:11,644] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN_STOP", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:11,794] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:11,896] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"eventType": 19, "addrType": 0, "addr": "80:6F:B0:EE:AD:32", "rssi": -62, "dataLen": 14, "data": "0A:08:52:54:4C:53:53:6C:61:76:65:02:01:06"}}
[2021-03-26 15:23:13,765] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN_STOP", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:13,868] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:13,970] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN", "payload": {"eventType": 19, "addrType": 0, "addr": "80:6F:B0:EE:AD:32", "rssi": -63, "dataLen": 14, "data": "0A:08:52:54:4C:53:53:6C:61:76:65:02:01:06"}}
[2021-03-26 15:23:15,840] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_SCAN_STOP", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:15,991] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_CONNECT", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:16,043] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_CONN_PARAMS", "payload": {"connHandle": 0, "accessAddress": 1447517676, "connInterval": 640, "hopValue": 9, "mSCA": 0, "currChan": 9, "chanMap": [255, 255, 255, 255, 31], "crcInit": 324548, "peerAddr": "80:6F:B0:EE:AD:32"}}
[2021-03-26 15:23:16,144] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_CONN_PARAMS", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:16,953] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_CONNECT", "payload": {"connHandle": 0, "status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:20,435] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_CONNECT", "payload": {"connHandle": 0, "status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:20,449] root -     INFO - Connection process done
[2021-03-26 15:23:20,537] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_IDENTIFY", "payload": {"capabilities": {"CM": true, "AOA_TX": false, "AOA_RX": true, "TOF_SLAVE": false, "TOF_PASSIVE": true, "TOF_MASTER": false, "RTLS_SLAVE": false, "RTLS_MASTER": false, "RTLS_PASSIVE": true}, "revNum": 2, "devId": "DeviceFamily_ID_CC26X2", "identifier": "80:6F:B0:31:D7:A8"}}
[2021-03-26 15:23:20,537] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_IDENTIFY", "payload": {"capabilities": {"CM": false, "AOA_TX": false, "AOA_RX": true, "TOF_SLAVE": false, "TOF_PASSIVE": false, "TOF_MASTER": true, "RTLS_SLAVE": false, "RTLS_MASTER": true, "RTLS_PASSIVE": false}, "revNum": 2, "devId": "DeviceFamily_ID_CC26X2", "identifier": "80:6F:B0:EE:9C:67"}}
[2021-03-26 15:23:20,637] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_SET_PARAMS", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:20,638] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_SET_PARAMS", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:20,650] root -     INFO - AOA Started
[2021-03-26 15:23:20,741] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_ENABLE", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:20,741] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_ENABLE", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:20,790] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_IDENTIFY", "payload": {"capabilities": {"CM": true, "AOA_TX": false, "AOA_RX": true, "TOF_SLAVE": false, "TOF_PASSIVE": true, "TOF_MASTER": false, "RTLS_SLAVE": false, "RTLS_MASTER": false, "RTLS_PASSIVE": true}, "revNum": 2, "devId": "DeviceFamily_ID_CC26X2", "identifier": "80:6F:B0:31:D7:A8"}}
[2021-03-26 15:23:20,792] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_IDENTIFY", "payload": {"capabilities": {"CM": false, "AOA_TX": false, "AOA_RX": true, "TOF_SLAVE": false, "TOF_PASSIVE": false, "TOF_MASTER": true, "RTLS_SLAVE": false, "RTLS_MASTER": true, "RTLS_PASSIVE": false}, "revNum": 2, "devId": "DeviceFamily_ID_CC26X2", "identifier": "80:6F:B0:EE:9C:67"}}
[2021-03-26 15:23:20,943] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_TOF_SET_PARAMS", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:21,250] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_TOF_SET_PARAMS", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:21,250] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": -23, "rssi": -57, "antenna": 1, "channel": 15}}
[2021-03-26 15:23:21,251] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": -23, "rssi": -80, "antenna": 1, "channel": 6}}
[2021-03-26 15:23:21,251] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 6}}
[2021-03-26 15:23:21,351] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_TOF_GET_SEC_SEED", "payload": {"seed": "0D:F5:65:D9:90:23:9E:A0:32:3E:76:B2:D4:36:02:7E:59:7A:B2:01:35:42:43:17:2B:52:D5:E5:B5:3C:F9:C9"}}
[2021-03-26 15:23:21,453] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_TOF_SET_SEC_SEED", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:21,505] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_TOF_CALIBRATE", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:21,565] root -     INFO - Calibration started in all passive nodes
[2021-03-26 15:23:21,566] root -     INFO - ToF started in all passive nodes
[2021-03-26 15:23:21,653] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_TOF_CALIBRATE", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:21,657] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_TOF_ENABLE", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:21,667] root -     INFO - Calibration started in master node
[2021-03-26 15:23:21,755] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_TOF_ENABLE", "payload": {"status": "RTLS_SUCCESS"}}
[2021-03-26 15:23:21,769] root -     INFO - ToF started in master node
[2021-03-26 15:23:22,008] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -69, "antenna": 1, "channel": 24}}
[2021-03-26 15:23:22,012] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": -27, "rssi": -79, "antenna": 1, "channel": 33}}
[2021-03-26 15:23:22,414] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": -30, "rssi": -78, "antenna": 1, "channel": 5}}
[2021-03-26 15:23:22,816] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -64, "antenna": 1, "channel": 5}}
[2021-03-26 15:23:22,819] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": -31, "rssi": -75, "antenna": 1, "channel": 14}}
[2021-03-26 15:23:23,221] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -60, "antenna": 1, "channel": 14}}
[2021-03-26 15:23:23,224] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": -32, "rssi": -85, "antenna": 1, "channel": 23}}
[2021-03-26 15:23:23,625] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -68, "antenna": 1, "channel": 23}}
[2021-03-26 15:23:24,032] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -57, "antenna": 1, "channel": 32}}
[2021-03-26 15:23:24,034] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": -13, "rssi": -76, "antenna": 1, "channel": 4}}
[2021-03-26 15:23:24,439] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 4}}
[2021-03-26 15:23:24,440] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": -6, "rssi": -75, "antenna": 1, "channel": 13}}
[2021-03-26 15:23:24,845] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -59, "antenna": 1, "channel": 13}}
[2021-03-26 15:23:24,845] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": -5, "rssi": -85, "antenna": 1, "channel": 22}}
[2021-03-26 15:23:25,198] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -70, "antenna": 1, "channel": 22}}
[2021-03-26 15:23:25,249] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 3, "rssi": -78, "antenna": 1, "channel": 31}}
[2021-03-26 15:23:25,603] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 24, "rssi": -75, "antenna": 1, "channel": 3}}
[2021-03-26 15:23:25,603] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -58, "antenna": 1, "channel": 31}}
[2021-03-26 15:23:26,009] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 3}}
[2021-03-26 15:23:26,009] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 36, "rssi": -76, "antenna": 1, "channel": 12}}
[2021-03-26 15:23:26,414] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 14, "rssi": -84, "antenna": 1, "channel": 21}}
[2021-03-26 15:23:26,414] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -59, "antenna": 1, "channel": 12}}
[2021-03-26 15:23:26,820] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -72, "antenna": 1, "channel": 21}}
[2021-03-26 15:23:26,820] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 29, "rssi": -78, "antenna": 1, "channel": 30}}
[2021-03-26 15:23:27,227] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -77, "antenna": 1, "channel": 2}}
[2021-03-26 15:23:27,227] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -59, "antenna": 1, "channel": 30}}
[2021-03-26 15:23:27,633] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 54, "rssi": -77, "antenna": 1, "channel": 11}}
[2021-03-26 15:23:27,634] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -66, "antenna": 1, "channel": 2}}
[2021-03-26 15:23:28,043] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 33, "rssi": -82, "antenna": 1, "channel": 20}}
[2021-03-26 15:23:28,043] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -60, "antenna": 1, "channel": 11}}
[2021-03-26 15:23:28,450] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 46, "rssi": -79, "antenna": 1, "channel": 29}}
[2021-03-26 15:23:28,450] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -72, "antenna": 1, "channel": 20}}
[2021-03-26 15:23:28,807] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 66, "rssi": -77, "antenna": 1, "channel": 1}}
[2021-03-26 15:23:28,807] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -62, "antenna": 1, "channel": 29}}
[2021-03-26 15:23:29,298] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 57, "rssi": -75, "antenna": 1, "channel": 10}}
[2021-03-26 15:23:29,299] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -81, "antenna": 1, "channel": 1}}
[2021-03-26 15:23:29,647] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 36, "rssi": -83, "antenna": 1, "channel": 19}}
[2021-03-26 15:23:29,655] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 48, "rssi": -61, "antenna": 1, "channel": 10}}
[2021-03-26 15:23:30,013] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -67, "antenna": 1, "channel": 19}}
[2021-03-26 15:23:30,053] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 47, "rssi": -78, "antenna": 1, "channel": 28}}
[2021-03-26 15:23:30,406] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 67, "rssi": -75, "antenna": 1, "channel": 0}}
[2021-03-26 15:23:30,421] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 28}}
[2021-03-26 15:23:30,810] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 59, "rssi": -80, "antenna": 1, "channel": 9}}
[2021-03-26 15:23:30,823] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -75, "antenna": 1, "channel": 0}}
[2021-03-26 15:23:31,216] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 37, "rssi": -80, "antenna": 1, "channel": 18}}
[2021-03-26 15:23:31,231] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -58, "antenna": 1, "channel": 9}}
[2021-03-26 15:23:31,620] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 48, "rssi": -79, "antenna": 1, "channel": 27}}
[2021-03-26 15:23:31,637] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 18}}
[2021-03-26 15:23:32,023] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 68, "rssi": -80, "antenna": 1, "channel": 36}}
[2021-03-26 15:23:32,043] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -66, "antenna": 1, "channel": 27}}
[2021-03-26 15:23:32,397] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -57, "antenna": 1, "channel": 36}}
[2021-03-26 15:23:32,428] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 44, "rssi": -88, "antenna": 1, "channel": 8}}
[2021-03-26 15:23:32,832] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 25, "rssi": -78, "antenna": 1, "channel": 17}}
[2021-03-26 15:23:32,852] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -58, "antenna": 1, "channel": 8}}
[2021-03-26 15:23:33,238] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 35, "rssi": -80, "antenna": 1, "channel": 26}}
[2021-03-26 15:23:33,257] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -60, "antenna": 1, "channel": 17}}
[2021-03-26 15:23:33,610] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -65, "antenna": 1, "channel": 26}}
[2021-03-26 15:23:33,641] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 57, "rssi": -82, "antenna": 1, "channel": 35}}
[2021-03-26 15:23:33,998] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 54, "rssi": -82, "antenna": 1, "channel": 7}}
[2021-03-26 15:23:34,016] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -56, "antenna": 1, "channel": 35}}
[2021-03-26 15:23:34,402] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 35, "rssi": -83, "antenna": 1, "channel": 16}}
[2021-03-26 15:23:34,422] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -61, "antenna": 1, "channel": 7}}
[2021-03-26 15:23:34,807] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 60, "rssi": -79, "antenna": 1, "channel": 25}}
[2021-03-26 15:23:34,826] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -60, "antenna": 1, "channel": 16}}
[2021-03-26 15:23:35,215] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 71, "rssi": -81, "antenna": 1, "channel": 34}}
[2021-03-26 15:23:35,234] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -65, "antenna": 1, "channel": 25}}
[2021-03-26 15:23:35,618] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 69, "rssi": -79, "antenna": 1, "channel": 6}}
[2021-03-26 15:23:35,639] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -56, "antenna": 1, "channel": 34}}
[2021-03-26 15:23:36,020] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 48, "rssi": -80, "antenna": 1, "channel": 15}}
[2021-03-26 15:23:36,044] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -62, "antenna": 1, "channel": 6}}
[2021-03-26 15:23:36,427] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 51, "rssi": -81, "antenna": 1, "channel": 24}}
[2021-03-26 15:23:36,448] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -59, "antenna": 1, "channel": 15}}
[2021-03-26 15:23:36,831] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -84, "antenna": 1, "channel": 33}}
[2021-03-26 15:23:36,852] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -65, "antenna": 1, "channel": 24}}
[2021-03-26 15:23:37,204] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -57, "antenna": 1, "channel": 33}}
[2021-03-26 15:23:37,233] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 45, "rssi": -77, "antenna": 1, "channel": 5}}
[2021-03-26 15:23:37,610] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 5}}
[2021-03-26 15:23:37,639] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 35, "rssi": -79, "antenna": 1, "channel": 14}}
[2021-03-26 15:23:38,014] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -58, "antenna": 1, "channel": 14}}
[2021-03-26 15:23:38,044] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 27, "rssi": -82, "antenna": 1, "channel": 23}}
[2021-03-26 15:23:38,419] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -66, "antenna": 1, "channel": 23}}
[2021-03-26 15:23:38,448] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 24, "rssi": -84, "antenna": 1, "channel": 32}}
[2021-03-26 15:23:38,803] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 19, "rssi": -75, "antenna": 1, "channel": 4}}
[2021-03-26 15:23:38,825] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -57, "antenna": 1, "channel": 32}}
[2021-03-26 15:23:39,206] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 21, "rssi": -78, "antenna": 1, "channel": 13}}
[2021-03-26 15:23:39,230] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -62, "antenna": 1, "channel": 4}}
[2021-03-26 15:23:39,609] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 0, "rssi": -81, "antenna": 1, "channel": 22}}
[2021-03-26 15:23:39,635] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -58, "antenna": 1, "channel": 13}}
[2021-03-26 15:23:40,016] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 22, "rssi": -83, "antenna": 1, "channel": 31}}
[2021-03-26 15:23:40,040] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -67, "antenna": 1, "channel": 22}}
[2021-03-26 15:23:40,422] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 28, "rssi": -75, "antenna": 1, "channel": 3}}
[2021-03-26 15:23:40,444] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -58, "antenna": 1, "channel": 31}}
[2021-03-26 15:23:40,798] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 3}}
[2021-03-26 15:23:40,827] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 48, "rssi": -77, "antenna": 1, "channel": 12}}
[2021-03-26 15:23:41,204] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -58, "antenna": 1, "channel": 12}}
[2021-03-26 15:23:41,607] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -71, "antenna": 1, "channel": 21}}
[2021-03-26 15:23:41,635] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 50, "rssi": -81, "antenna": 1, "channel": 30}}
[2021-03-26 15:23:42,012] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -59, "antenna": 1, "channel": 30}}
[2021-03-26 15:23:42,040] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 71, "rssi": -75, "antenna": 1, "channel": 2}}
[2021-03-26 15:23:42,417] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 2}}
[2021-03-26 15:23:42,444] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 86, "rssi": -78, "antenna": 1, "channel": 11}}
[2021-03-26 15:23:42,823] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -58, "antenna": 1, "channel": 11}}
[2021-03-26 15:23:42,850] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 62, "rssi": -80, "antenna": 1, "channel": 20}}
[2021-03-26 15:23:43,205] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 65, "rssi": -79, "antenna": 1, "channel": 29}}
[2021-03-26 15:23:43,228] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -81, "antenna": 1, "channel": 20}}
[2021-03-26 15:23:43,610] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 68, "rssi": -77, "antenna": 1, "channel": 1}}
[2021-03-26 15:23:43,633] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -62, "antenna": 1, "channel": 29}}
[2021-03-26 15:23:44,014] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 62, "rssi": -79, "antenna": 1, "channel": 10}}
[2021-03-26 15:23:44,039] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -71, "antenna": 1, "channel": 1}}
[2021-03-26 15:23:44,420] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 53, "rssi": -86, "antenna": 1, "channel": 19}}
[2021-03-26 15:23:44,444] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -59, "antenna": 1, "channel": 10}}
[2021-03-26 15:23:44,824] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 61, "rssi": -78, "antenna": 1, "channel": 28}}
[2021-03-26 15:23:44,851] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -75, "antenna": 1, "channel": 19}}
[2021-03-26 15:23:45,229] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 81, "rssi": -77, "antenna": 1, "channel": 0}}
[2021-03-26 15:23:45,253] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 28}}
[2021-03-26 15:23:45,607] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -74, "antenna": 1, "channel": 0}}
[2021-03-26 15:23:45,634] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 74, "rssi": -79, "antenna": 1, "channel": 9}}
[2021-03-26 15:23:46,012] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -59, "antenna": 1, "channel": 9}}
[2021-03-26 15:23:46,039] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 53, "rssi": -85, "antenna": 1, "channel": 18}}
[2021-03-26 15:23:46,416] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -67, "antenna": 1, "channel": 18}}
[2021-03-26 15:23:46,443] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 61, "rssi": -80, "antenna": 1, "channel": 27}}
[2021-03-26 15:23:46,821] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 27}}
[2021-03-26 15:23:46,849] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 70, "rssi": -78, "antenna": 1, "channel": 36}}
[2021-03-26 15:23:47,202] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 68, "rssi": -86, "antenna": 1, "channel": 8}}
[2021-03-26 15:23:47,225] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -57, "antenna": 1, "channel": 36}}
[2021-03-26 15:23:47,605] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 48, "rssi": -84, "antenna": 1, "channel": 17}}
[2021-03-26 15:23:47,631] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -60, "antenna": 1, "channel": 8}}
[2021-03-26 15:23:48,010] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 56, "rssi": -78, "antenna": 1, "channel": 26}}
[2021-03-26 15:23:48,037] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 17}}
[2021-03-26 15:23:48,414] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 78, "rssi": -80, "antenna": 1, "channel": 35}}
[2021-03-26 15:23:48,445] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -65, "antenna": 1, "channel": 26}}
[2021-03-26 15:23:48,799] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -56, "antenna": 1, "channel": 35}}
[2021-03-26 15:23:48,819] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 77, "rssi": -84, "antenna": 1, "channel": 7}}
[2021-03-26 15:23:49,205] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -61, "antenna": 1, "channel": 7}}
[2021-03-26 15:23:49,224] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 57, "rssi": -81, "antenna": 1, "channel": 16}}
[2021-03-26 15:23:49,608] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -60, "antenna": 1, "channel": 16}}
[2021-03-26 15:23:49,629] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 60, "rssi": -79, "antenna": 1, "channel": 25}}
[2021-03-26 15:23:50,014] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -65, "antenna": 1, "channel": 25}}
[2021-03-26 15:23:50,034] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 78, "rssi": -81, "antenna": 1, "channel": 34}}
[2021-03-26 15:23:50,420] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -56, "antenna": 1, "channel": 34}}
[2021-03-26 15:23:50,440] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 76, "rssi": -80, "antenna": 1, "channel": 6}}
[2021-03-26 15:23:50,795] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 55, "rssi": -79, "antenna": 1, "channel": 15}}
[2021-03-26 15:23:50,824] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -63, "antenna": 1, "channel": 6}}
[2021-03-26 15:23:51,200] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 58, "rssi": -81, "antenna": 1, "channel": 24}}
[2021-03-26 15:23:51,229] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -59, "antenna": 1, "channel": 15}}
[2021-03-26 15:23:51,604] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 54, "rssi": -85, "antenna": 1, "channel": 33}}
[2021-03-26 15:23:51,632] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 49, "rssi": -65, "antenna": 1, "channel": 24}}
[2021-03-26 15:23:51,935] root -     INFO - MASTER: 80:6F:B0:EE:9C:67 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_IDENTIFY", "payload": {"capabilities": {"CM": false, "AOA_TX": false, "AOA_RX": true, "TOF_SLAVE": false, "TOF_PASSIVE": false, "TOF_MASTER": true, "RTLS_SLAVE": false, "RTLS_MASTER": true, "RTLS_PASSIVE": false}, "revNum": 2, "devId": 255, "identifier": "02:FA:10:10:02:F9"}}
[2021-03-26 15:23:51,959] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "SyncRsp", "subsystem": "RTLS", "command": "RTLS_CMD_IDENTIFY", "payload": {"capabilities": {"CM": true, "AOA_TX": false, "AOA_RX": true, "TOF_SLAVE": false, "TOF_PASSIVE": true, "TOF_MASTER": false, "RTLS_SLAVE": false, "RTLS_MASTER": false, "RTLS_PASSIVE": true}, "revNum": 2, "devId": "DeviceFamily_ID_CC26X2", "identifier": "80:6F:B0:31:D7:A8"}}
[2021-03-26 15:23:51,966] root -     INFO - AOA Stopped
[2021-03-26 15:23:52,010] root -     INFO - PASSIVE: 80:6F:B0:31:D7:A8 --> {"originator": "Nwp", "type": "AsyncReq", "subsystem": "RTLS", "command": "RTLS_CMD_AOA_RESULT_ANGLE", "payload": {"connHandle": 0, "angle": 51, "rssi": -77, "antenna": 1, "channel": 5}}
[2021-03-26 15:24:22,101] werkzeug -     INFO - 192.168.137.74 - - [26/Mar/2021 15:24:22] "GET /send/3 HTTP/1.1" 500 -

十分期待您的回复。

  • 首先声明一下:
    作为蓝牙®低能耗(BLE)解决方案的供应商,我们致力于提供高质量的协议栈,重点放在互操作性和广泛的市场应用上。

    在以前的软件开发套件(SDK)中,TI在实验的基础上引入了一种新的创新测距技术,称为飞行时间(ToF)和我们的BLE协议栈作为软件示例,以演示新测距技术的一种可能选择。此ToF示例技术基于私有扩展,仅演示了兼容TI设备之间的操作。

    不同供应商和系统之间的互操作性是至关重要的价值,TI倾听了这一市场和客户的需求。展望未来,TI已决定将我们的安全测距工作合并到标准化解决方案中,重点放在广泛的适应性和互操作性上。

    作为专注于标准化解决方案的决定的一部分,TI决定终止对SDK中TI专有ToF软件示例的进一步开发和支持。

    同时,我们将重点放在为安全测距技术创建标准上,并打算在这些解决方案可用时转换现有技术。

    TOF技术目前尚未被纳入蓝牙联盟标准SPEC,TI在SDK3.40之后版本中取消了关于TOF的内容,之后也不再提供技术支持

  • 终止进一步的开发和支持针对的是3.4之后的版本,但当前的3.3和3.4版本应该是能做到AoA和TOF并行展示的,所以我还是想问下,现阶段有没有办法能够解决我在3.4版本所遇到的上述问题,正常后续版本的更迭应该不影响之前的SDK版本的使用。
    我当前的项目研究可能需要在AOA角度之上去获取额外的TOF信息,所以想要实现这个效果,希望尊敬的工作人员能够给与我解答。
    或者正如您所说,TI将专注于标准化解决方案(而不是之前TOF仅针对TI设备私有),那么现阶段在CC26X2开发板上是否有可用的安全测距技术的例程?
    十分期待您的回复!
  • TOF例程演示参考这里dev.ti.com/.../node
    标准化解决方案是指符合蓝牙联盟标准,目前没有测距例程,只有AOA
  • 好的,通过上述连接,我明白了TOF无法在Passive正常运行的原因是我外附了BOOSTXL-AOA天线板。

    那么我是否可以,在修改Passive的 TOF_passive = false(能告诉我在哪里修改这个吗?),仅允许master去进行TOF测量。这样我就可以同时获得1.AOA值(BOOSTXL-AOA在passive端获取的值)2.TOF值(仅依靠Master端获取)

    我不知道这样的操作是否有文件说明指导,还是说在SDK3.3或者3.4下,必须由三个Langchpad且不应该有任何的BOOSTXL-AOA附置,不能仅依靠Master端去测量TOF。

    十分期待你的回复。
  • 是的,TOF和AOA不能同时使用,TOF必须使用三个Langchpad板载天线,不应该有任何的BOOSTXL-AOA