This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工具:CCS10.4
协议栈为CCS上最新的5_20_00_52
app:安卓 Simplelink Starter_v5.7.3
由于CC2642内存较大,想要放弃片外OAD,尝试使用片上OAD。了解到相关说明,需要构建三个项目bim_onchip , persistent_app , simple_peripheral_oad_onchip.
使用Flash Programmer 2 下载了三个程序,下载后可以在Simplelink Starter APP上找到蓝牙广播为 SP OAD on-chip,连接复位后显示蓝牙广播为OAD persistent App.此时连接升级,选择文件后,加载后似乎只传播了一包数据就停止不动,可以看到卡在Current Speed:403b/s。
我发现,如果只下载bim_onchip , persistent_app ,可以连接升级,但是会卡在98%不动。
现在下载三个程序反而不行,请求指导一下。
究其原因是构建_oad.bin文件失败,先前使用的是ccs10.3是可行的,现在更新为10.4后无法自动生成,且原有的在ccs10.3的off-chip片外的OAD项目导入后也无法生成_oad.bin文件,该如何是好?退回10.3版本还是有其他解决办法?
makefile:219: recipe for target 'post-build' failed
make (e=193): Error 193
gmake[2]: [post-build] Error 193 (ignored)
以下为生成的情况
C:/ti/simplelink_cc13x2_26x2_sdk_5_20_00_52/tools/common/oad/oad_image_tool --verbose ccs D:/xxx/CCS104/persistent_app_CC26X2R1_LAUNCHXL_tirtos_ccs 0 -hex1 Release/persistent_app_CC26X2R1_LAUNCHXL_tirtos_ccs.hex -k C:/ti/simplelink_cc13x2_26x2_sdk_5_20_00_52/tools/common/oad/private.pem -o Release/persistent_app_CC26X2R1_LAUNCHXL_tirtos_ccs_oad
makefile:219: recipe for target 'post-build' failed
process_begin: CreateProcess(C:\ti\simplelink_cc13x2_26x2_sdk_5_20_00_52\tools\common\oad\oad_image_tool, C:/ti/simplelink_cc13x2_26x2_sdk_5_20_00_52/tools/common/oad/oad_image_tool --verbose ccs D:/xxx/CCS104/persistent_app_CC26X2R1_LAUNCHXL_tirtos_ccs 0 -hex1 Release/persistent_app_CC26X2R1_LAUNCHXL_tirtos_ccs.hex -k C:/ti/simplelink_cc13x2_26x2_sdk_5_20_00_52/tools/common/oad/private.pem -o Release/persistent_app_CC26X2R1_LAUNCHXL_tirtos_ccs_oad, ...) failed.
make (e=193): Error 193
gmake[2]: [post-build] Error 193 (ignored)
感谢回复。我尝试回到10.3,发现问题还是存在,然后把协议栈5_20_00_52 降回之前可以使用的5.10.00.48,发现问题不存在。怀疑跟协议栈有关,不知道您有没有尝试使用这个版本的,确认下是否哪里出现问题。
现在可以升级,但是还是有些异常,
1:SP OAD on-chip在安卓手机设置复位,启动OAD后,重启手机蓝牙和APP,广播依然搜索到为SP OAD on-chip,需要连接一次后(此时连接会出现异常)重新刷新蓝牙才会更新为OAD persistent App,且显示OAD persistent App后连接方可成功连接上设备,为何呢?如果只是广播手机缓存问题,重启蓝牙和重启APP,应该是可以解决的,但问题似乎不是这样。
2:如果我切换为OAD persistent App状态后,不想升级了,如何返回到SP OAD on-chip状态?重启设备还是无效