This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC1352R1: watchdog timer的clock來源?

Part Number: LAUNCHXL-CC1352R1


sdk:simplelink_cc13xx_cc26xx_sdk_6_10_00_29

請問watchdog timer的clock來源是從哪裡來的? 是RTC嗎?

在datasheet上面看到watchdog timer是1.5MHz clock rate, 這個是從哪一個clock source來的? (SCLK_HF?SCLK_MF?SCLK_LF?)

"The watchdog timer runs on a 1.5 MHz clock rate and cannot be stopped once enabled. The watchdog timer pauses to run in Standby power mode and when a debugger halts the device."

  • 您好,

    收到您的问题了,我们升级到英文论坛给工程师看下,有答复尽快给到您。

  • 您好,

    从文档SWCU185E(CC13x2, CC26x2 SimpleLink Wireless MCU Technical Reference Manual): https://www.ti.com/lit/ug/swcu185e/swcu185e.pdf?ts=1661307320327&ref_url=https%253A%252F%252Fe2e.ti.com%252F可以了解到相应信息:

    • The WDT is running off the INFRASTRUCTURE clock sourced by the MCU Power, Reset, and Clock Management (PRCM) module.
    • ...MCU_AON has two clocks, an INFRASTRUCTURE clock that always runs and a PERBUSULL clock that is identical to the INFRASTRUCTURE clock whenever the SYSBUS clock is running...INFRASTRUCTURE and PERBUSULL clocks are automatically controlled to run at a maximum of half the clock frequency of SCLK_HF, regardless of the settings in PRCM:INFCLKDIVR.RATIO, PRCM:INFCLKDIVS.RATIO, or PRCM:INFCLKDIVDS.RATIO.
    • 5.2.3 Scaler to WDT
      There is a scaler with a fixed-division ratio of 32 of the MCU clock that is present. Regardless of the settings
      in the PRCM:INFCLKDIVR, the PRCM:INFCLKDIVS, and the PRCM:INFCLKDIVDS registers, the watchdog
      counts at a constant speed.

    所以1.5 MHz是来自 48 MHz (HF)去除以 32。

    希望能够帮助到您。