This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: 一主两从通信,对从机抓包,发现有重复包和异常包现象。

Part Number: CC2640R2F


2个从机发送notify数据给主机,相距10cm左右。通过wireshark抓从机的包,数据包中有记录发送包的个数的参数:00-ff。

通过空中抓包数据分析发现有重复包现象,以及 异常包现象。请问这可能是什么造成的?该怎么解决?

两个从机设置的最小连接间隔最大 连接间隔都是25ms。

53.322ms时包序是cc,

53.347ms时包序是cd,                 //时间差25ms,连接间隔正常

53.373ms时包序是ce。                  //时间差26ms,连接间隔是否正常

53.423ms时包序是cf;                   //时间差50ms,连接间隔异常

53.451ms时包序是cf;                   //时间差28ms,连接间隔异常,数据发两次

53.452ms时包序是d0;                  //时间差1ms,连接间隔异常,数据正常

53.472ms时包序是d1;                  //时间差20ms,连接间隔异常,数据正常

53.497ms时包序是d2;                    //时间差25ms,连接间隔正常,数据正常

53.522ms时包序是d3;                    //时间差25ms,连接间隔正常,数据正常

56.497ms时包序是46;

56.522ms时包序是47;                    //时间差25ms,

56.546ms时包序是48;                    //时间差24ms,

56.571ms时包序是49;                    //时间差25ms,

56.597ms时包序是4A;                    //时间差26ms,

56.625ms时包序是4A;                    //时间差28ms, 数据重发

56.626ms时包序是4B;                    //时间差1ms,

56.647ms时包序是4C;                    //时间差21ms,

56.672ms时包序是4D;                    //时间差25ms,

56.696ms时包序是4E;                    //时间差24ms,

数据异常:上一个包序是4B,中间是68,下一个包是4C