This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: 使用CCS导入一个BLE5-stack例程simple_central,调用GapScan_enable(0, DEFAULT_SCAN_DURATION, 0)后程序死掉

Part Number: CC2640R2F

如题,SDK版本是SimpleLink CC2640R2 SDK - 4.30.00.08.

我在程序中添加了看门狗,发现调用GapScan_enable后过一段时间程序就复位了。

可以确定硬件是没有问题的,我有一个老的工程SDK版本是simplelink_cc2640r2_sdk_1_40_00_45工作正常。

我初始化了串口,通过串口接收一个指令后调用SimpleCentral_doDiscoverDevices开始扫描,程序执行到GapScan_enable就死了

我已经附上了代码。simple_central.csimple_central.h

/***********************************************************************//**
 * @file       SerialInterface.c
 * @brief      
 * @details    
 * @author     Nick ( Nick.yao@justec.cn )
 * @version    
 * @date       2023-02-23 14:08:25
 * @pre        
 * @copyright  Copyright <span style="font-family:Microsoft Sans Serif;">&copy; </span>Nick ( Nick.yao@justec.cn ). All rights reserved.
 */
#include "SerialInterface.h"
#include "Att.h"

//#include "Protocol.h"
//#include "Crc.h"

//#include "peripheral.h"
//#include "devinfoservice.h"
//#include "simpleGATTprofile.h"
//#include "simpleBLEPeripheral.h"

#include "hci.h"

#include <ti/drivers/UART.H>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>

#include "Board.h"
#include "OSAL.h"
#include <stdio.h>
#include <string.h>


//2018-4-10
#include "gatt.h"

//#include "simpleGATTprofile.h"
#include "simple_gatt_profile.h"

//2018-5-17
#include "simple_central.h"

#include "LinkList.h"

//2018-5-17
extern uint8 simpleBLEState;




static UART_Handle      hUART;
static Semaphore_Handle hUARTSem;
static Semaphore_Struct sUARTSem;

static Task_Struct      sUARTTask;

#define UART_TASK_STACK_SIZE                  (512u)
#define UART_TASK_PRIORITY                    (1u)
Char UART_TaskStack[UART_TASK_STACK_SIZE];

//2018-4-24
static uint8_t   rxBuf[256];
//static uint8_t   rxBuf[5000];

static uint16_t  rxWRAddr = 0;
static uint16_t  rxRDAddr = 0;

static uint8_t   rxBuf2[256];

_transMode transMode = eCTRL_MODE;

void SerialReadCallback( UART_Handle handle, void *buf, size_t count );
void SerialWriteCallback( UART_Handle handle, void *buf, size_t count );

int SerialSend( UART_Handle handle, void *buf, size_t count );
int SerialRead( UART_Handle handle, void *buf, size_t count );

void SerialTaskFxn( UArg a0, UArg a1 );

void ProtocolForBulk();
void ProtocolForCTRL();
void BluetoothSwitch( bool val );

extern void SerialBulkEvent( _transMode mode );

//2018-3-23
//void Uart_SendMsg(uint8 cmd,uint8 data);

//2018-3-26
static uint8 sendMsgTo_TaskID;


uint8 timeoutFlag;

uint8 disconnectFlag;



//2018-5-11

#include <xdc/runtime/Assert.h>
#include <xdc/runtime/Types.h>
#include <xdc/runtime/Log.h>
#include <ti/sysbios/BIOS.h>
#include "board.h"
#include <ti/drivers/power/PowerCC26XX.h>
#include <ti/drivers/UART.h>
#include <ti/drivers/uart/UARTCC26XX.h>
/*********************�궨��************************/
#if defined(CC2640R2DK_7ID)
#define GUA_UART_RX IOID_1 //��������
#define GUA_UART_TX IOID_2 //��������
#else
#define GUA_UART_RX IOID_0 //��������
#define GUA_UART_TX IOID_1 //��������
#endif
//#define CC2640R2DK_4XS_UART_RX                       IOID_0          	/* P1.7 */
//#define CC2640R2DK_4XS_UART_TX                       IOID_1          	/* P1.9 */

/*********************�ڲ�����************************/
//���ں�
typedef enum{
GUA_UART0 = 0,
GUA_UARTCOUNT
}GUA_UARTName;
//���������������
const UARTCC26XX_HWAttrsV2 GUA_UART_CC26XXHWAttrs[GUA_UARTCOUNT] = {
{
.baseAddr = UART0_BASE,
.powerMngrId = PowerCC26XX_PERIPH_UART0,
.intNum = INT_UART0_COMB,
.intPriority = ~0,
.swiPriority = 0,
.txPin = GUA_UART_TX,
.rxPin = GUA_UART_RX,
.ctsPin = PIN_UNASSIGNED,
.rtsPin = PIN_UNASSIGNED
}
};
//����Ŀ��
static UARTCC26XX_Object GUA_UART_CC26XXObjects[GUA_UARTCOUNT];
static const UART_Config GUA_UART_Config[GUA_UARTCOUNT] = {
{
.fxnTablePtr = &UARTCC26XX_fxnTable,
.object = &GUA_UART_CC26XXObjects[GUA_UART0],
.hwAttrs = &GUA_UART_CC26XXHWAttrs[GUA_UART0]
},
};
//���ھ��
static UART_Handle stGUA_UART_Handle;
//���ڲ���
static UART_Params stGUA_UART_Params;

#define GUA_UART_MAX_NUM_RX_BYTES 60 //�������ֽ�
#define GUA_UART_MAX_NUM_TX_BYTES 60 //������ֽ�

/*********************�ⲿ����************************/
uint8 gaGUA_UART_RxBuf[GUA_UART_MAX_NUM_RX_BYTES] = {0};
uint8 gaGUA_UART_TxBuf[GUA_UART_MAX_NUM_TX_BYTES] = {0};
uint32 gGUA_UART_WantedRxBytes;
uint8 gGUA_UART_Size;

///////////////////////////////////////////////////////
#define USE_LINK_LIST 1
#if (USE_LINK_LIST == 1)
typedef struct _ts_voc_data{
	LinkListNode next;
	uint16_t voc;
	uint16_t temp;
	uint16_t humi;
	uint8_t  status;
	uint8_t  rev;
}TS_VOC_DATA;
#else
typedef struct _ts_voc_data{
	uint16_t voc;
	uint16_t temp;
	uint16_t humi;
	uint8_t  status;
	uint8_t  rev;
}TS_VOC_DATA;
#endif

#define VOC_BUF_LEN 90


TS_VOC_DATA voc_data[VOC_BUF_LEN];


LinkList *idle_list,*data_list;



static float HexToFloat(uint8_t *buf)
{
	union{
	float t;
	uint8_t    ndata[4];
	}tmp;

	tmp.ndata[3] = buf[0];
	tmp.ndata[2] = buf[1];
	tmp.ndata[1] = buf[2];
	tmp.ndata[0] = buf[3];

	return tmp.t;
}


static uint16_t U16LittleToBig(uint16_t val)
{
	union{
		uint16_t t;
		uint8_t  ndata[2];
	}tmp,ret;
	tmp.t = val;
	ret.ndata[0] = tmp.ndata[1];
	ret.ndata[1] = tmp.ndata[0];
	return ret.t;
}


static void set_up_link_list(void)
{
	int i;
	idle_list = LinkList_Creat();
	data_list = LinkList_Creat();
	for(i=0; i<VOC_BUF_LEN; i++){
		LinkList_Insert(idle_list,(LinkListNode*)&voc_data[i],0);
	}
}





#if (USE_LINK_LIST == 1)
void voc_data_puts(uint8_t* dataflow)
{
	TS_VOC_DATA *p;
	float t;

	if(LinkList_Length(idle_list) > 0){
		p = (TS_VOC_DATA *)LinkList_Delete(idle_list, 0);//�ӿ�������õ�һ��buf
	}else{
		p = (TS_VOC_DATA *)LinkList_Delete(data_list, 0);//�����������н���ɵ�����ɾ��
	}

	memcpy((uint8_t*)&(p->voc), dataflow, 2);
	t = HexToFloat(dataflow+2);
	p->temp = U16LittleToBig((uint16_t)(t*10));
	t = HexToFloat(dataflow+6);
	p->humi = U16LittleToBig((uint16_t)(t*10));
	p->status = dataflow[10];
	LinkList_Insert(data_list, (LinkListNode *)p, LinkList_Length(data_list));//�������������
}

static uint8_t voc_datas_output(TS_VOC_DATA* p)
{
	uint8_t ret = 0;
	TS_VOC_DATA *pdata;

	if(LinkList_Length(data_list) > 0){
		pdata = (TS_VOC_DATA *)LinkList_Delete(data_list, 0);//�����������н���ɵ������ͳ�
		p->voc = pdata->voc;
		p->temp = pdata->temp;
		p->humi = pdata->humi;
		p->status = pdata->status;
		LinkList_Insert(idle_list,(LinkListNode*)pdata,0);//�����нڵ����
		ret = 1;
	}

	return ret;
}
#else
static uint16_t voc_read = 0, voc_write = 0;
void voc_data_puts(uint8_t* dataflow)
{
	float t;
	memcpy((uint8_t*)&(voc_data[voc_write].voc), dataflow, 2);
	t = HexToFloat(dataflow+2);
	voc_data[voc_write].temp = U16LittleToBig((uint16_t)(t*10));
	t = HexToFloat(dataflow+6);
	voc_data[voc_write].humi = U16LittleToBig((uint16_t)(t*10));
	voc_data[voc_write].status = dataflow[10];
	voc_write++;
	if(voc_write >= VOC_BUF_LEN) voc_write = 0;
}

static uint8_t voc_datas_output(TS_VOC_DATA* p)
{
	uint8_t ret = 0;
	if(voc_read != voc_write){
		p->voc = voc_data[voc_read].voc;
		p->temp = voc_data[voc_read].temp;
		p->humi = voc_data[voc_read].humi;
		p->status = voc_data[voc_read].status;
		voc_read++;
		if(voc_read >= VOC_BUF_LEN) voc_read = 0;
		ret = 1;
	}
	return ret;
}

#endif

//2018-5-7
//���ھ��
//���������ݳ���
/*
#define GUA_UART_MAX_NUM_RX_BYTES 60 //�������ֽ�
#define GUA_UART_MAX_NUM_TX_BYTES 60 //������ֽ�

static UART_Handle stGUA_UART_Handle;
uint8 gaGUA_UART_RxBuf[GUA_UART_MAX_NUM_RX_BYTES] = {0};
uint8 gaGUA_UART_TxBuf[GUA_UART_MAX_NUM_TX_BYTES] = {0};
uint32 gGUA_UART_WantedRxBytes;
uint8 gGUA_UART_Size;
*/

//void SerialInit()
void SerialInit(__UART_Callback SerialReadCallback)
{
    UART_Params      params;
    Semaphore_Params sParams;
    Task_Params      TaskParams;

	set_up_link_list();
    
    HCI_EXT_SetTxPowerCmd( HCI_EXT_TX_POWER_5_DBM );
       
    /* io config in Board.c */
    
    /* uart config */
    UART_Params_init(&params);
    
    /* 57600, N, 8, 1 */
   params.baudRate  = 115200;
//    params.baudRate  = 230400;

    params.parityType = UART_PAR_NONE;
    params.dataLength = UART_LEN_8;
    params.stopBits = UART_STOP_ONE;
    
    params.readMode = UART_MODE_CALLBACK;
    params.readCallback = SerialReadCallback;
    
    params.writeMode = UART_MODE_BLOCKING;
    params.writeCallback = NULL;
    
    params.writeDataMode = UART_DATA_BINARY;
    params.readDataMode = UART_DATA_BINARY;
    
    params.readReturnMode = UART_RETURN_FULL;
    params.readEcho = UART_ECHO_OFF;
    
    /* Initialize the UART driver */
    UART_init();

//2018-4-4
//   hUART = UART_open( CC2650_UART0, &params );
//	hUART = UART_open( Board_UART0, &params );


	stGUA_UART_Handle =
	GUA_UART_Config[0].fxnTablePtr->openFxn((UART_Handle)&GUA_UART_Config[0],
	&params);


	//������ھֲ����ع���
	GUA_UART_Config[0].fxnTablePtr->controlFxn(stGUA_UART_Handle,
	UARTCC26XX_CMD_RETURN_PARTIAL_ENABLE, NULL);

    
 /*  
    Semaphore_Params_init( &sParams );
    sParams.mode = Semaphore_Mode_BINARY;
    
    Semaphore_construct( &sUARTSem, 0, &sParams );
    hUARTSem = Semaphore_handle( &sUARTSem );
    
    
    Task_Params_init( &TaskParams );
    TaskParams.stack      = UART_TaskStack;
    TaskParams.stackSize  = UART_TASK_STACK_SIZE;
    TaskParams.priority   = UART_TASK_PRIORITY;
    
    Task_construct( &sUARTTask, SerialTaskFxn, &TaskParams, NULL );
*/

	gGUA_UART_WantedRxBytes = GUA_UART_MAX_NUM_RX_BYTES;
//	GUA_UART_Config[0].fxnTablePtr->readFxn(stGUA_UART_Handle,gaGUA_UART_RxBuf, gGUA_UART_WantedRxBytes);
//    SerialRead( hUART, &rxBuf2[0], 1);
	SerialRead(stGUA_UART_Handle,gaGUA_UART_RxBuf, gGUA_UART_WantedRxBytes);
}

void SerialDeinit()
{
  if( NULL != hUART )
  {
    UART_readCancel( hUART );
    
    UART_close( hUART );
    
    Task_destruct( &sUARTTask );
  }
}

int SerialSend( UART_Handle handle, void *buf, size_t count )
{
  int ret;
  
  ret = UART_write( handle, buf, count );
  
  return ret;
}

int SerialRead( UART_Handle handle, void *buf, size_t count )
{
  int ret;
  
 // ret = UART_read( handle, buf, count );

  ret =	GUA_UART_Config[0].fxnTablePtr->readFxn(handle,buf, count);

  return ret;
}

//2018-4-24
//int SerialSendSimple( void *buf, size_t count )
int SerialSendSimple( void *buf, uint16_t count )

{
  int ret;
   //2018-5-11 
  if( NULL != stGUA_UART_Handle )
  	  ret =	GUA_UART_Config[0].fxnTablePtr->writeFxn(stGUA_UART_Handle,buf, count );
//    if( NULL != hUART )
//    ret = UART_write( hUART, buf, count );
  
  return ret;
}

int DBG_Print(void *buf, uint16_t count)
{
//	return SerialSendSimple(buf,count);
	return 0;
}


void SerialReadCallback( UART_Handle handle, void *buf, size_t count )
{
  size_t i;

  
  for( i = 0; i < count; i ++ )
  {
    rxBuf[ rxWRAddr ++ ] = ( ( uint8_t * )buf )[ i ];
    
    if( sizeof( rxBuf ) <= rxWRAddr )   rxWRAddr = 0;
  }
  
//  Semaphore_post( hUARTSem );

	GUA_UART_Config[0].fxnTablePtr->readFxn(stGUA_UART_Handle,gaGUA_UART_RxBuf, gGUA_UART_WantedRxBytes);

}

//void SerialWriteCallback( UART_Handle handle, void *buf, size_t count )
//{
//  
//}

uint8_t SerialGetRxData()
{
  uint8_t ret;
  
  if( rxRDAddr != rxWRAddr )
  {
    ret = rxBuf[ rxRDAddr ++ ];
  }
  else{} //!< equal
  
  if( sizeof( rxBuf ) <= rxRDAddr )   rxRDAddr = 0;
  
  return ret;
}

void  SerialGetRxBuf(uint8 *buf, uint16 len)
{
  uint8_t i;

  for(i=0;i<len;i++)
	*buf++ = SerialGetRxData();

}


//2018-4-24
//uint8_t SerialGetRxLen()
uint16_t SerialGetRxLen()
{
  if( rxRDAddr != rxWRAddr )
  {
    return ( ( rxWRAddr > rxRDAddr ) ? ( rxWRAddr - rxRDAddr ) : ( sizeof( rxBuf ) - rxRDAddr + rxWRAddr ) );
  }
  
  return 0;
}

void SerialReceiveProcess()
{
  switch( transMode )
  {
  case eCTRL_MODE:
    ProtocolForCTRL();
    break;
    
  case eBULK_MODE:
    ProtocolForBulk();
    break;
    
  default:
    break;
  }
}

void SerialTaskFxn( UArg a0, UArg a1 )
{
  /* init task */


  for (;;)
  {
//2018-5-11  
//    SerialRead( hUART, &rxBuf2[0], 1 );
	GUA_UART_Config[0].fxnTablePtr->readFxn(stGUA_UART_Handle,gaGUA_UART_RxBuf, gGUA_UART_WantedRxBytes);
    Semaphore_pend( hUARTSem, BIOS_WAIT_FOREVER );


 //2018-4-11
    // receive process 
//    SerialReceiveProcess();
  }

  
}

void ProtocolForBulk()
{  
//  if( 20 <= SerialGetRxLen() )
//    SerialBulkEvent( transMode );
}


typedef struct
{
  uint8_t u8DatNo;
   uint8_t u8Data[26]; 
   
}_AlcoPrint_Data;

_AlcoPrint_Data *pAlcoPrint_Data;


void ProtocolForCTRL()
{

  static uint8_t lastDat = 0;
  static uint8_t frameBeginFlag = FALSE;
  static uint8_t frameLength = 0;
  static uint8_t tmpBuf[64];
  static uint8_t tmpBufCnt;
  
  uint8_t  curDat;
  uint8_t  checksum[2];

//2018-3-19
/*   
  curDat = SerialGetRxData();
  
  if( TRUE == frameBeginFlag )
  {
    if( 0 != frameLength )
    {
      tmpBuf[tmpBufCnt ++] = curDat;
      
      frameLength --;
      
      if(frameLength == 0) //receive all data complete
      {
         frameBeginFlag = FALSE;
         
         GenerateChecksum( checksum, 0, tmpBuf, tmpBuf[2] - 2 );
              
         if( ( tmpBuf[tmpBuf[2] - 1] == checksum[1] ) && 
            ( tmpBuf[tmpBuf[2] - 2] == checksum[0] ) )
         {
           switch( tmpBuf[3] )
           {
           case 0x14:  //!< ready or not?
             if( ( 0x07 == tmpBuf[2] ) && ( 0x01 == tmpBuf[4] ) )
             {
             }
             break;
             
           case 0x88:  //!< mode
             if( 0x07 == tmpBuf[2]  )
             {
               BluetoothSwitch( ON );
               
//               transMode = ( _transMode )tmpBuf[4];
               
               GenerateChecksum( tmpBuf, tmpBuf[2] - 2, tmpBuf, tmpBuf[2] - 2 );
               
               SerialSendSimple( tmpBuf, tmpBuf[2] );      
             }
             break;
             
           case 0x04:  //!< swver
             if( ( 0x07 == tmpBuf[2] ) && ( 0x05 == tmpBuf[4] ) )
             {                    
               DevInfo_GetParameter( DEVINFO_SOFTWARE_REV, tmpBuf + 5 );
               
               tmpBuf[2] = 0x0F;
               
               GenerateChecksum( tmpBuf, tmpBuf[2] - 2, tmpBuf, tmpBuf[2] - 2 );
                              
               SerialSendSimple( tmpBuf, tmpBuf[2] );
               
             }
             break;
             
           default:
             break;
           }
         }
      }
    }
    else
    {
      if( curDat > 5 ) //length of frame
      {
        frameLength = curDat - 3;
        
        tmpBufCnt = 0;
        
        tmpBuf[tmpBufCnt ++] = 0xfa;
        tmpBuf[tmpBufCnt ++] = 0xf5;
        tmpBuf[tmpBufCnt ++] = curDat;
      }
      else
      {
        frameBeginFlag = FALSE; 
      }
    }
  }
  else
  {
    if( ( 0xFA == lastDat ) && ( 0xF5 == curDat ) )
    {
      frameBeginFlag = TRUE;
    }
  }
  
  lastDat = curDat;
  
 */
  attWriteReq_t AttReq;

  curDat = SerialGetRxData();

//  tmpBuf[tmpBufCnt++] = curDat;
	AttReq.pValue[tmpBufCnt++] = curDat;
  if(tmpBufCnt>=20)
  {
 //2018-4-10

//	memcpy(&AttReq.pValue,tmpBuf,tmpBufCnt);

	AttReq.handle = charHdl +1 ;// 0x0035;//0xFFE9;//simpleBLECharHdl;
	AttReq.len =tmpBufCnt;//20;// SIMPLEPROFILE_CHAR6_LEN;

	AttReq.sig = 0;
	AttReq.cmd = 0;
	GATT_WriteNoRsp( simpleBLEConnHandle, &AttReq );
/***************************/

//  	SerialSendSimple(tmpBuf,tmpBufCnt);
	tmpBufCnt = 0;
  }

}


//static uint8 beginFlag = 0;
 uint8 beginFlag = 0;





void ProtocolForCTRL2()
{

  static uint8 frameStart;
  static uint8 frameCount;




  if( beginFlag )
  {
//    attHandleValueNoti_t nData;
//    attWriteReq_t AttReq;
	
    uint16 recLen = SerialGetRxLen();
    uint16 len = 0;


	if(recLen)
	{
/*		len = ( recLen > SIMPLEPROFILE_CHAR6_LEN ) ? SIMPLEPROFILE_CHAR6_LEN : recLen;
//		AttReq.value[0] = len;
		HalUARTRead (port, AttReq.value, len);
//		if(strstr(AttReq.value,Ptinter_FrameEnd)==NULL)
		{
			AttReq.handle = simpleBLECharHdl +1;// 0x0035;//0xFFE9;//simpleBLECharHdl;
	//		AttReq.len =SIMPLEPROFILE_CHAR6_LEN;//20;// SIMPLEPROFILE_CHAR6_LEN;
			AttReq.len =len;//20;// SIMPLEPROFILE_CHAR6_LEN;

			AttReq.sig = 0;
			AttReq.cmd = 0;
	//		osal_memcpy(&AttReq.value[1],nData.value,nData.len);
	//		osal_memcpy(AttReq.value,nData.value,nData.len);
			GATT_WriteCharValue( 0, &AttReq, simpleBLETaskId );

//			HalUARTWrite(HAL_UART_PORT_1,AttReq.value, len);
		}
*/		
	}
	    
  }

  else
  {
    if ( SerialGetRxLen() >= 8 )
    {
//      (void)SerialRead (port, pAlcoPrint_Data->u8Data, 1);
	      SerialRead( hUART, pAlcoPrint_Data->u8Data, 1);

//        (void)HalUARTRead (port, pAlcoPrint_Data->u8Data, 26);
    
      if( pAlcoPrint_Data->u8Data[0] == 0x1b )
      {
//       (void)HalUARTRead (port, pAlcoPrint_Data->u8Data + 1, 25);
	      SerialRead( hUART, pAlcoPrint_Data->u8Data+ 1, 7);
        
        if((pAlcoPrint_Data->u8Data[6] == 0x0d) && (pAlcoPrint_Data->u8Data[7] == 0x0a))
        {
          if((pAlcoPrint_Data->u8Data[0] == 0x1b) && (pAlcoPrint_Data->u8Data[1] == 0x40) && 
             (pAlcoPrint_Data->u8Data[4] == 0x1b) && (pAlcoPrint_Data->u8Data[5] == 0x40))
          {
            beginFlag = 1;
            
//            Uart_SendMsg(UART_Conn,0);
            
            pAlcoPrint_Data->u8DatNo = 0;   
            
//           timeoutFlag = TRUE;
            
//            osal_start_timerEx( sendMsgTo_TaskID, 4, 1 );
          }
        }
      }
      else
      {
        return;
      }
    }
  }
}

/*
//void Uart_SendMsg(uint8 cmd,uint8 data)
void Uart_SendMsg(uint8_t event, uint8_t state)
{
//  sappPacket_t *msgPkt;
  
  msgPkt = (sappPacket_t *)osal_msg_allocate( sizeof(sappPacket_t) );
  
  if ( msgPkt )
  {
    msgPkt->hdr.event = UART_MESSAGE;
    msgPkt->cmd  = cmd;
    msgPkt->data = data;
   
    osal_msg_send( sendMsgTo_TaskID, (uint8 *)msgPkt );
  }
//

//  sbpEvt_t *pMsg;

  // Create dynamic pointer to message.
  if ((pMsg = ICall_malloc(sizeof(sbpEvt_t))))
  {
    pMsg->hdr.event = event;
    pMsg->hdr.state = state;

    // Enqueue the message.
    Util_enqueueMsg(appMsgQueue, sem, (uint8*)pMsg);
  }
//
  
}
*/


/*
void BluetoothSwitch( bool val )
{
    uint8_t advertising;

    gaprole_States_t gapRole_state;
    
    GAPRole_GetParameter( GAPROLE_STATE, &gapRole_state );
    GAPRole_GetParameter( GAPROLE_ADVERT_ENABLED, &advertising );

    // terminates the existing connection 
    if( OFF == val )    
    {
        if( gapRole_state == GAPROLE_CONNECTED )
        {
            GAPRole_TerminateConnection();
        }
      
        if( OFF != advertising )
        {
          advertising = OFF;
          
          // turn off advertising 
          GAPRole_SetParameter( GAPROLE_ADVERT_ENABLED, sizeof( uint8_t ), &advertising );
        }
    }
    else
    {
        if( ( gapRole_state != GAPROLE_CONNECTED ) && ( ON != advertising ) )
        {
            advertising = ON;
            // turn on advertising 
            GAPRole_SetParameter( GAPROLE_ADVERT_ENABLED, sizeof( uint8_t ), &advertising );
        }
    }
}

*/


uint8 EstablishLink_Idx,EstablishLink_Flag;
uint8 Scan_Flg ;


#define TOTAL_COMMAND  4
char arCommand[TOTAL_COMMAND][10] = {"SCAN0","SCAN1","DISCONNET","CONNET"};
int FindCommand(uint8 *szCommand)
{
    char *p;	
    uint8  command;
    uint8	offset;

    for( int i = 0 ; i < TOTAL_COMMAND ; i ++)
    {
    	  p = strstr(szCommand,&arCommand[i][0]) ;
        if(p!= NULL )
        {
           switch(i)
           {
		case 0 ://SCAN0
				//Uart_SendMsg(UART_Disconn);
				SimpleCentral_doStopDiscovering(0);
				break;
		case 1 ://SCAN1
	 	          //Uart_SendMsg(UART_Start);
	 	          //SerialSendSimple("start discovery\r\n",17);
	 	          SimpleCentral_doDiscoverDevices(0);
	 		      break;
		case 2 ://DISCONNET
			      beginFlag = 0;
	 	            Uart_SendMsg(UART_Terminate);			

				break;
		case 3 ://CONNET
				if (simpleBLEState != BLE_STATE_CONNECTED)
				{

                    command =(p[6]-0x30)*10;
					command += (p[7]-0x30);
					if(command<=scanRes)
					{

						EstablishLink_Idx = command;
						Uart_SendMsg(UART_Conn);
						EstablishLink_Flag = 1;
					}
					else
					{
						
					}
				}
				break;	
				
	      		default:
      				break;
           }

	     break;		
        }
    }
}



char tttxBuf[64];

void BLEProcessBulkEvent( )
{
  uint8_t txBuf[64];
  uint16_t txBufLen, i;
  uint16_t rxBufLen = SerialGetRxLen();
  
  uint16 timeOut;
  
  char* command;
      uint8_t status;


//2018-6-1

	if(rxBufLen>0)
	{

		if( rxBufLen > 20 ) txBufLen = 20;
		else                txBufLen = rxBufLen;

		SerialGetRxBuf (txBuf, txBufLen);

		command=strstr(txBuf,"AT+");

		if(command != NULL)
		{
			FindCommand(command+3);
			return;
		}
	}



	if( beginFlag )
	{


	    if( rxBufLen )
	    {
			attWriteReq_t AttReq;
			//FA F5 00 14 90
//			if(txBuf[0] == 0xfa && txBuf[1] == 0xf5 && txBuf[4] == 0x90){
//				uint8_t title_end[4] = {0x1b,0x40,0x1b,0x40};
//				uint8_t send_temp[7];
//				TS_VOC_DATA p;
//				SerialSendSimple(title_end,4);
//				while(voc_datas_output(&p)){
//					memcpy(send_temp, (uint8_t*)&(p.voc), 7);
//					SerialSendSimple(send_temp,7);
//				}
//				SerialSendSimple(title_end,4);
//			}
//			else
			{


				AttReq.pValue = GATT_bm_alloc(simpleBLEConnHandle, ATT_WRITE_REQ, txBufLen, NULL);

				if ( AttReq.pValue != NULL )
				{
					AttReq.handle = charHdl+1;
					AttReq.len = txBufLen;

					AttReq.sig = 0;
					//2018-4-24
					//		          AttReq.cmd = 0;
					AttReq.cmd = 1;

					//				  SerialGetRxBuf(AttReq.pValue,txBufLen);
					memcpy(AttReq.pValue,txBuf,txBufLen);

					//2018-4-24
					//		          status = GATT_WriteCharValue(simpleBLEConnHandle, &AttReq, selfEntity);
					status =  GATT_WriteNoRsp(simpleBLEConnHandle, &AttReq);
					char pbuf[30];
					sprintf(pbuf,"Send tick:%d\r\n",Clock_getTicks());
					DBG_Print(pbuf,strlen(pbuf));

					if ( status != SUCCESS )
					{
						GATT_bm_free((gattMsg_t *)&AttReq, ATT_WRITE_REQ);
					}

				}
			}
		}
	}
}








/*
    if( rxBufLen )
    {
      if( rxBufLen > 20 ) txBufLen = 20;
      else                txBufLen = rxBufLen;
      
      for( i = 0; i < txBufLen; i ++ )
        txBuf[i] = SerialGetRxData();
      
      timeOut = 0;
      
//      IS_READY( timeOut, ( SimpleProfile_SetParameter( CUSTOM_NOTIFICATION, txBufLen, &txBuf[0] ) != SUCCESS ) );
		memcpy(&AttReq.pValue,txBuf,txBufLen);

		AttReq.handle = charHdl +1;// 0x0035;//0xFFE9;//simpleBLECharHdl;
		AttReq.len =txBufLen;//20;// SIMPLEPROFILE_CHAR6_LEN;

		AttReq.sig = 0;
		AttReq.cmd = 0;
		GATT_WriteCharValue( 0, &AttReq, selfEntity );


    }

*/

//2018-4-8
/*
	if( beginFlag )
	{


	    if( rxBufLen )
	    {
  		attWriteReq_t AttReq;

		
	      if( rxBufLen > CUSTOM_DATA_TRANSFER_LEN ) txBufLen = CUSTOM_DATA_TRANSFER_LEN;
	      else                txBufLen = rxBufLen;


		AttReq.pValue = GATT_bm_alloc(simpleBLEConnHandle, ATT_WRITE_REQ, txBufLen, NULL);
		  
//		SerialGetRxBuf(txBuf, txBufLen);
//		command=strstr(txBuf,"AT+");

		SerialGetRxBuf(AttReq.pValue,txBufLen);
		command=strstr(AttReq.pValue,"AT+");	
	
		if(command!=NULL)
		{
			FindCommand(command+3);
		}
		else
		{
		        if ( AttReq.pValue != NULL )
		        {
		          AttReq.handle = charHdl+1;
		          AttReq.len = txBufLen;
//			    memcpy(AttReq.pValue,txBuf,txBufLen);

		          AttReq.sig = 0;
//2018-4-24
//		          AttReq.cmd = 0;
		          AttReq.cmd = 1;

//2018-4-24
//		          status = GATT_WriteCharValue(simpleBLEConnHandle, &AttReq, selfEntity);
			   status =  GATT_WriteNoRsp(simpleBLEConnHandle, &AttReq);
		          if ( status != SUCCESS )
		          {
		            GATT_bm_free((gattMsg_t *)&AttReq, ATT_WRITE_REQ);
		          }
				  
		        }
		}




	    }
	}
	else
	{


		if(rxBufLen>0)
		{
			SerialGetRxBuf (txBuf, rxBufLen);
			command=strstr(txBuf,"AT+");

			if(command!=NULL)
			{
				FindCommand(command+3);
			}
		}
	}
	
}
*/
SerialInterface.h