This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-CC2652R7: ImmediateCmd :CMD_MODIFY_FS 命令执行的条件?

Part Number: LP-CC2652R7

int ModifyChannel(RF_Handle rfHandle,uint8_t channel){
   
    rfc_CMD_MODIFY_FS_t cmdModifyFs ={
        .commandNo = CMD_MODIFY_FS,
        .frequency = 2400 + channel,
        .fractFreq = 0
    };

    uint32_t start_tm = RF_getCurrentTime();
    RF_Stat status = RF_runImmediateCmd(rfHandle, (uint32_t*)&cmdModifyFs);
    if(RF_StatSuccess == status){
        uint32_t diff = RF_getCurrentTime() - start_tm; 
        printf("Modify TO CHN:%d use %d us\n",channel,(diff+3)/4);
    }else{
        RF_printCmdStat(status);
    }
    return (int)status;
}

我尝试了一下如上面的代码,系统老是返回:RF_StatInvalidParamsError,

想问一下这个命令执行前提是什么?是RF_postCmd RX或TX后异步执行?

希望您能指导一下。

  • 您好,

    我们需要一点时间查看这个问题,有结论后及时联系您。

  • 谢谢您的回复

    RF_printCmdStat 仅仅是打印了枚举值

    void RF_printCmdStat(RF_Stat result){
        if(result == RF_StatBusyError)          {printf("RF_StatBusyError\n");return ;}
        if(result == RF_StatRadioInactiveError) {printf("RF_StatRadioInactiveError\n");return ;}
        if(result == RF_StatCmdDoneError)       {printf("RF_StatCmdDoneError\n");return ;}
        if(result == RF_StatInvalidParamsError) {printf("RF_StatInvalidParamsError\n");return ;}
        if(result == RF_StatCmdEnded)           {printf("RF_StatCmdEnded\n");return ;}
        if(result == RF_StatError)              {printf("RF_StatError\n");return ;}
        if(result == RF_StatCmdDoneSuccess)     {printf("RF_StatCmdDoneSuccess\n");return ;}
        if(result == RF_StatCmdSch)             {printf("RF_StatCmdSch\n");return ;}
        if(result == RF_StatSuccess)            {printf("RF_StatSuccess\n");return ;}
        printf("Unknow:%d\n",result)  ;
    }
    

  • 您好,

    您的这部分代码是有在相关SDK示例中吗?

  • 不是,都自己写的,

    调用ModifyChannel 之前已确定radio 已经打开并 FS了。send & recv 都OK。

  • 您好,

    RF_cancelCmd返回RF_StatInvalidParamsError。

    可以参考一下easylink_abort函数实现里对RF_cancelCmd参数的检查。

    EasyLink_Status EasyLink_abort(void)
    {
        EasyLink_Status status = EasyLink_Status_Cmd_Error;
        if ( (!configured) || suspended)
        {
            return EasyLink_Status_Config_Error;
        }
        //check an Async command is running, if not return success
        if (!EasyLink_CmdHandle_isValid(asyncCmdHndl))
        {
            return EasyLink_Status_Aborted;
        }
        //force abort (gracefull param set to 0)
        if (RF_cancelCmd(rfHandle, asyncCmdHndl, 0) == RF_StatSuccess)
        {
            /* If command is cancelled immediately, callback may have set the cmd handle to invalid.
             * In that case, no need to pend.
             */
            if (EasyLink_CmdHandle_isValid(asyncCmdHndl))
            {
                /* Wait for Command to complete */
                RF_EventMask result = RF_pendCmd(rfHandle, asyncCmdHndl, (RF_EventLastCmdDone |
                        RF_EventCmdAborted | RF_EventCmdCancelled | RF_EventCmdStopped));
                if (result & RF_EventLastCmdDone)
                {
                    status = EasyLink_Status_Success;
                }
            }
            else
            {
                /* Command already cancelled */
                status = EasyLink_Status_Success;
            }
        }
        else
        {
            status = EasyLink_Status_Cmd_Error;
        }
        return status;
    }

  • 谢谢回复,

    我的問题是为什么 RF_runImmediateCmd ( 命令号:CMD_MODIFY_FS) 总是返回 RF_StatInvalidParamsError

    或如何正确使用 CMD_MODIFY_FS命令,最好有相关示例,谢谢

  • 您好,

    您可以参考 Radio Software Bundle (rflib) APIs  similar E2E threads,但没有具体的CMD_MODIFY_FS示例。

    首先,您应确保在更改频率之前关闭无线电(RF_yield)。然后,CMD_MODIFY_FS命令本身仅用于较小的频率变化(几MHz)以保持PLL lock,所以channel更改不适用于这种情况。考虑到这个用例,我们认为应该使用CMD_FS,并使用RF_runCmd而不是RF_runImmediateCmd。