This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: 自制开发板使用CCS烧录提示error:unable to access device register

Part Number: CC2640R2F

参考官方原理图自制的CC2640R2F核心板,原理图如下

使用XDS110仿真器进行下载,提示Error connecting to the target:
(Error -2131 @ 0x0)
Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 7.0.48.0)

测VDDS电压3.23V,VDDR电压2.23V

  • 您好,

    您可以查看一下该链接:Device register。其中有说到此错误意味着 JTAG 调试器无法访问电路板上的内核或设备,从技术上讲,JTAG 调试器无法访问 ICEPick 寄存器。

    您可否先按连接中的提示排除一下相应的硬件问题?

  • 您好,感谢回复

    我检查了TMS,TCK,TDO,TDI,RST的连接都没有问题。

    我在ccs中修改ccxml配置为4-pin standard mode时提示Error connecting to the target: (Error -242 @ 0x0) A router subpath could not be accessed. The board configuration file is probably incorrect. (Emulation package 7.0.48.0)

    配置为2-pin mode时提示Error connecting to the target:(Error -2131 @ 0x0)Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).(Emulation package 7.0.48.0)

    尝试用smartRF flash programmer 2进行forced mass erase也失败了,提示

    看到数据手册上面VDDR的电压值在1.7-1.95V,我的VDDR在2.2V左右,请问这个有关系吗?

  • 您好,

    看到数据手册上面VDDR的电压值在1.7-1.95V,我的VDDR在2.2V左右,请问这个有关系吗?

    这个不能确定是否与该问题有直接联系,但是还是想要您将VDDR保持在推荐值之内,以防出现不可控的问题。

  • 我尝试更换芯片都出现了这样的问题(VDDR和DCOUPL电压高过参考电压),怀疑是不是和结构布局有关系,能不能麻烦您看一下布局是否有误呢?

  • 您好,

    麻烦您可以在以下链接申请相应的硬件审核:SIMPLELINK-2-4GHZ-DESIGN-REVIEWS,有专业的硬件工程师帮您查看相应硬件问题。

    感谢您的支持。