Part Number: LAUNCHXL-CC26X2R1
UART读数据为回调方式,当串口输入数据时,并没有效果
//UART读取回调函数。修改灯状态
void uart_read_datdCB(UART2_Handle handle, void *buf, size_t count, void *userArg, int_fast16_t status)
{
static int flag = 0;
flag = ~flag;
GPIO_write(CONFIG_GPIO_LED, flag);
}
//UART初始化
void uart_init2(void)
{
UART2_Params params;
UART2_Params_init(¶ms);
params.baudRate = 115200;
params.writeMode = UART2_Mode_BLOCKING;
params.readMode = UART2_Mode_CALLBACK;
params.readCallback = &uart_read_datdCB;
// Open the UART
uart = UART2_open(CONFIG_UART2_0_CONST, ¶ms);
if (uart == NULL) {
// UART2_open() failed
while (1);
}
// Enable receiver, inhibit low power mode
UART2_rxEnable(uart);
uint8_t buffer_tmp[] = "UART2 init ok\r\n";
UART2_write(uart, buffer_tmp, sizeof(buffer_tmp), NULL);
}