Part Number: CC2640
我目前在基于CC2640F128做一个蓝牙遥控器项目,一个模块做主机,一个做从机。经常有这种现象。原先两个设备正常烧录可以正常配对和绑定,也可以正常通信。但是如果将从设备重新烧录固件,一模一样的固件。出现二者不断连接,又断开。提示REASON 22的错误。并且两个设备重新断电重启都没有用。然后将主机或者从机重新烧录或者随便改一点无关的代码,重新烧录就又大概率的OK了。这种原因大概什么呢?由于这种现象很随机,并且,一模一样的固件,或者固件稍微改点又行了。但过一会重新烧一下又不行了。
部分参数设置如下:
// Maximum number of scan responses
#define DEFAULT_MAX_SCAN_RES 8
// Scan duration in ms
#define DEFAULT_SCAN_DURATION 4000
// How often to perform periodic event (in msec)
#define SBP_PERIODIC_EVT_PERIOD 500
// Discovery mode (limited, general, all)
#define DEFAULT_DISCOVERY_MODE DEVDISC_MODE_ALL
// TRUE to use active scan
#define DEFAULT_DISCOVERY_ACTIVE_SCAN TRUE
// TRUE to use white list during discovery
#define DEFAULT_DISCOVERY_WHITE_LIST FALSE
// TRUE to use high scan duty cycle when creating link
#define DEFAULT_LINK_HIGH_DUTY_CYCLE FALSE
// TRUE to use white list when creating link
#define DEFAULT_LINK_WHITE_LIST FALSE
// Default RSSI polling period in ms
#define DEFAULT_RSSI_PERIOD 1000
// Whether to enable automatic parameter update request when a connection is
// formed
#define DEFAULT_ENABLE_UPDATE_REQUEST GAPCENTRALROLE_PARAM_UPDATE_REQ_AUTO_ACCEPT
// Minimum connection interval (units of 1.25ms) if automatic parameter update
// request is enabled
#define DEFAULT_UPDATE_MIN_CONN_INTERVAL 400
// Maximum connection interval (units of 1.25ms) if automatic parameter update
// request is enabled
#define DEFAULT_UPDATE_MAX_CONN_INTERVAL 1200
// Slave latency to use if automatic parameter update request is enabled
#define DEFAULT_UPDATE_SLAVE_LATENCY 0
// Supervision timeout value (units of 10ms) if automatic parameter update
// request is enabled
#define DEFAULT_UPDATE_CONN_TIMEOUT 600
// Default passcode
#define DEFAULT_PASSCODE 19655
// Default GAP pairing mode
#define DEFAULT_PAIRING_MODE GAPBOND_PAIRING_MODE_INITIATE
// Default MITM mode (TRUE to require passcode or OOB when pairing)
#define DEFAULT_MITM_MODE TRUE
// Default bonding mode, TRUE to bond
#define DEFAULT_BONDING_MODE TRUE
// Default GAP bonding I/O capabilities
#define DEFAULT_IO_CAPABILITIES GAPBOND_IO_CAP_DISPLAY_ONLY
// Default service discovery timer delay in ms
#define DEFAULT_SVC_DISCOVERY_DELAY 1000
// TRUE to filter discovery results on desired service UUID
#define DEFAULT_DEV_DISC_BY_SVC_UUID TRUE
// Length of bd addr as a string
#define B_ADDR_STR_LEN 15
// Task configuration
#define SBC_TASK_PRIORITY 1
#ifndef SBC_TASK_STACK_SIZE
#define SBC_TASK_STACK_SIZE 864
#endif