Part Number: LP-EM-CC2340R5
Other Parts Discussed in Thread: CC2340R5
定义OAD_IMG_ID_VAL部分,没有找到DeviceFamily_ID_CC23X0R5相关的,是这个头文件在CC2340R5里没用了,还是SDK代码没有更新?
#if defined(DeviceFamily_CC26X2) || defined (DeviceFamily_CC26X2_V2) || \
defined(DeviceFamily_CC26X2X7) || defined(DeviceFamily_CC26X1)
#define OAD_IMG_ID_VAL {'C', 'C', '2', '6', 'x', '2', 'R', '1'}
#elif defined (DeviceFamily_CC13X2) || \
defined (DeviceFamily_CC13X2X7) || \
defined (DeviceFamily_CC13X1) || \
defined (DeviceFamily_CC13X2_V1) || \
defined (DeviceFamily_CC13X2_V2)
#define OAD_IMG_ID_VAL {'C', 'C', '1', '3', 'x', '2', 'R', '1'}
#elif defined (DeviceFamily_CC13X4)
#define OAD_IMG_ID_VAL {'C', 'C', '1', '3', 'x', '4', ' ', ' '}
#elif defined (DeviceFamily_CC26X3)
#define OAD_IMG_ID_VAL {'C', 'C', '2', '6', 'x', '3', ' ', ' '}
#elif defined (DeviceFamily_CC26X4)
#define OAD_IMG_ID_VAL {'C', 'C', '2', '6', 'x', '4', ' ', ' '}
#elif defined (DeviceFamily_CC26X0R2)
#define OAD_IMG_ID_VAL {'O', 'A', 'D', ' ', 'I', 'M', 'G', ' '}
#elif defined (DOXYGEN)
/*!
* Magic number to identify OAD image header. It is recommended that the
* customer adjust these to uniquely identify their device
*
* This define will be filled in conditionally based on DeviceFamily_*
* - DeviceFamily_CC26X2: @code {'C', 'C', '2', '6', 'x', '2', 'R', '1'} @endcode
* - DeviceFamily_CC13X2: @code {'C', 'C', '1', '3', 'x', '2', 'R', '1'} @endcode
* - DeviceFamily_CC26X0R2: @code {'O', 'A', 'D', ' ', 'I', 'M', 'G', ' '} @endcode
* - Else an error will be thrown
*/
#define OAD_IMG_ID_VAL
#else
#error "Unknown Device Family"
#endif //DeviceFamily_CC26X2