This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-EM-CC2340R5: oad_image_header.h中没有CC2340R5?

Part Number: LP-EM-CC2340R5
Other Parts Discussed in Thread: CC2340R5

定义OAD_IMG_ID_VAL部分,没有找到DeviceFamily_ID_CC23X0R5相关的,是这个头文件在CC2340R5里没用了,还是SDK代码没有更新?

#if defined(DeviceFamily_CC26X2) || defined (DeviceFamily_CC26X2_V2) || \
    defined(DeviceFamily_CC26X2X7) || defined(DeviceFamily_CC26X1)
  #define OAD_IMG_ID_VAL                    {'C', 'C', '2', '6', 'x', '2', 'R', '1'}
#elif defined (DeviceFamily_CC13X2) ||                                        \
      defined (DeviceFamily_CC13X2X7) ||                                      \
      defined (DeviceFamily_CC13X1) ||                                        \
      defined (DeviceFamily_CC13X2_V1) ||                                     \
      defined (DeviceFamily_CC13X2_V2)
  #define OAD_IMG_ID_VAL                    {'C', 'C', '1', '3', 'x', '2', 'R', '1'}
#elif defined (DeviceFamily_CC13X4)
  #define OAD_IMG_ID_VAL                    {'C', 'C', '1', '3', 'x', '4', ' ', ' '}
#elif defined (DeviceFamily_CC26X3)
  #define OAD_IMG_ID_VAL                    {'C', 'C', '2', '6', 'x', '3', ' ', ' '}
#elif defined (DeviceFamily_CC26X4)
  #define OAD_IMG_ID_VAL                    {'C', 'C', '2', '6', 'x', '4', ' ', ' '}
#elif defined (DeviceFamily_CC26X0R2)
  #define OAD_IMG_ID_VAL                    {'O', 'A', 'D', ' ', 'I', 'M', 'G', ' '}
#elif defined (DOXYGEN)
  /*!
   * Magic number to identify OAD image header. It is recommended that the
   * customer adjust these to uniquely identify their device
   *
   * This define will be filled in conditionally based on DeviceFamily_*
   *   - DeviceFamily_CC26X2:  @code {'C', 'C', '2', '6', 'x', '2', 'R', '1'} @endcode
   *   - DeviceFamily_CC13X2:  @code {'C', 'C', '1', '3', 'x', '2', 'R', '1'} @endcode
   *   - DeviceFamily_CC26X0R2: @code {'O', 'A', 'D', ' ', 'I', 'M', 'G', ' '} @endcode
   *   - Else an error will be thrown
   */
  #define OAD_IMG_ID_VAL
#else
  #error "Unknown Device Family"
#endif //DeviceFamily_CC26X2