This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: RTLS界面AOA数据不变,BOOSTXL-AOAx1, CC26X2R1 x3 ,SDK4.20

Part Number: LAUNCHXL-CC26X2R1


硬件CC26X2R  x3 

BOOSTXL-AOA  x1

sdk 4.20

将BOOSTXL连接到passive上,运行后运行的ui界面如图所示,我已经移动了很多次板子了,但是他的aoa始终为50左右

我已经完成的工作有:1、将passive的天线切换到外置天线 2、已经下载了master、passive、slaver固件,并且已经下载.out文件到硬件中 3、已经试过将带有天线板的cc26改成master并且生成的图像的aoa也是固定到50左右一直不变。

问题:想知道怎么才能实现aoa测量的ui界面正常侧相

  • 运行ui界面的时候我用示波器测了dio的四个端口

    只有DIO27和DIO29是高电平3.3v,所以一直都是天线A1.1,并且不切换,这样肯定就得不到aoa数据(因为aoa的测量需要天线的切换),请问我的问题出在哪里