This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: IQ数据的处理

Part Number: LAUNCHXL-CC26X2R1


专家您好,

1、这是我收集到的IQ数据,采用的是sdk5.10,使用AOA—boostxl天线板,使用的是两个天线A1.1、A1.2进行切换,然后采集到的IQ数据这么大正常吗?

2、另外,依然用sdk5.10与AOA-boostxl。把天线A1.1与A1.2IQ数据按照下图1的方式处理,并把A1.1与A1.2的计算的角度值相减=相位差,而相位差的图如下图2,为什么相位差超过了-180~180这个范围?

  • 专家您好,另外补充几点疑问

    3、左边是官方提供的图,图中(phase,6)(phase,14).......与我右图运行出来的(phase,7)(phase,8)......这些通道好像不一样,这是随机抽取通道产生的图吗?

  • 1.看起来数据是有些不太正常,仍是此前所说的,要注意减小干扰

    2.这个角度范围指的是一对IQ数据算出来的角度,不是相位差的范围,如果绘制连续的IQ数据图,它应该是类正弦波

    3.这是根据自己的测试情况确定的,不一样没有问题

  • 专家您好:

    我用的是三块cc2642的发射板,一块AOA-boostxl,将AOAboostxl搭载在发射板上作为passive  

    1、我用5.30sdk采集到的天线数据有passive与coordinator的两份原始IQ数据,为什么两份数据不一样?coodinator的IQ数据是passive传给它的吧?

    2、为什么IQ数据中的每个pkt 中的sample_idx只采集了45组?(0-44)这个45是由什么决定的?

    3、收集到的IQ数据中,这个pkt有时候都到178了,我可以不要那么多吗?我可以自己设置吗?

    4、我用的天线切换就用两个天线[0,1],下图一就是我不同时间在同一地点同一个角度采集IQ数据,结果却发现IQ数据采集到的总数目不一样。coodinator有采了4410组、4455组,这是为什么?

    5、与问题4一样的,passive采集到的IQ数据总数也不一致,有采了3870组、3600组、3460组。这是为什么?

    6、上述1-5问题的情况是我用sdk5.30采集的IQ数据发现的疑问,我用skd5.20做相同的实验的时候,得到的IQ数据一会只有一份coodinetor的IQ数据,一会又passive与coodinatore都齐全,这是什么原因导致一会一份一会两份?

    7、使用sdk5.20时,接受到的coodinator的IQ数据总数也不一样有四百多组的有七百多组的,这总数不应该是512组吗?

    8、我如果使用4MHz 、2us的插槽,且是过滤后IQ数据,采集到的IQ数据有包含参考周期(8us)、天线切换周期(2us)和天线稳定期(1us)中的数据吗?

    恳求专家解惑,再次感激!

  • 请为此重开一个新帖,以便其他工程师查看