Part Number: TRF7970A
目前使用TRF7970A开发P2P模式,我查看了TRF7970A数据手册和peer to peer communication with trf7970A,我手上有两块TRF7970A板子,一个板子作为INITIATOR,另一块板子作为TARGET。现在我想实现active communication。我流程如下:首先初始化两块板子,ISO control register 为0x21,然后根据手册上说的,对INITIATOR板子先进行RF初始化碰撞,确定没有RF磁场时,打开RF场,开启传输命令,并将字节长度输入到TX_LENGTH_BYTE_1和TX_LENGTH_BYTE_2寄存器中,再将数据写入到FIFO寄存器,此时测量INITIATOR上TX引脚,有出现震荡波,是否已经开始发送?那么对另一块TARGET接收,我的流程应该是怎么样的?如何才能接收到INITIATOR发出来的数据