CC1310: F128RSMR

Part Number: CC1310

在设计cc1310硬件设计,

1.未找到bootloader模式选择的对应的上拉引脚吗,在初始化时debug模式需要更改mcu模式还想用默认的?

2.晶振在烧录后测试抓取不到波形,这是在初始化需要设置晶振的引脚工作的时候才能测出波形吗?

3.在使用ccs对应的cc1310f128案例,单板是32引脚,案例是48引脚。对应的**.h文件需要修改gpio口个数及定义吗,以及adc定义吗?

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 您好

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待

  • 您好

    1.有关引导加载程序的更多信息,请参阅www.ti.com/.../swcu117

    2.您是否试图在帽阵列调谐后测量晶体频率?

    3.应定义所有gpio端口

  • 1.所以,可以不设bootloader引脚,在软件中设置模式。
    2.外部晶振不起振不影响程序的初始化吗?本身内部有rtc来工作就可以加载吗?我看32k用于低功耗开启,24Mhz用于射频
    3.在没有使用spi i2c urt 串口引脚,不需要使用加密,只使用ido5一个adc采样引脚。仍要把定义10个io口,删除多出的引脚,才能初始化工作吗?

  • 我使用了32引脚的单板,并未修改程序中任何引脚定义。在debug时出现的问题报错
    Current optimization/debug settings:  --opt_level=off  --opt_for_speed=1    -g
    Detecting compilation without optimization. Recommend setting --opt_level=3. NOTE: debug ability will decrease.

    Not all available code size is being used. Recommend running Optimization Assistant to find best speed vs size setting (--opt_for_speed). Double-click to start.

    如果想跑最小系统的,urt spi iic rf 加密 看门狗是否都可以注释掉。io口引脚能去除吗?还是要将48引脚一一对应到32引脚端口

  • 您好

    请发布您的示意图,以便审核。晶体通常不会失效。实际上,32kHz用于低功率模式,24MHz用于RF。

  • 已检查过,晶振需要打开配置才能工作。但是现在在烧录过程中使用空例程,在烧录过程中一次能烧录下一次就不能烧录,第3次就又可以烧录。间隔性烧录,所以使用的空例程中软件需要配置什么吗?什么原因引起的这个问题。这是硬件的设计   。是有引脚错误吗?或者软件需要引导程序