利用CC1310例程两个任务的原代码,jlink下载不能实现多任务的切换,不知道什么原因
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
多任务的基本结构就是在main函数里启动任务初始化函数
例如:
int main(void)
{
/* Call board init functions. */
Board_initGeneral();
/* Open LED pins */
ledPinHandle = PIN_open(&ledPinState, pinTable);
if(!ledPinHandle) {
System_abort("Error initializing board LED pins\n");
}
//add by barbara -- begin
/* Open Button pins */
buttonPinHandle = PIN_open(&buttonPinState, buttonPinTable);
if (!buttonPinHandle) {
System_abort("Error initializing button pins\n");
}
//add by barbara -- end
//System_printf("main\n");
/* Clear LED pins */
PIN_setOutputValue(ledPinHandle, Board_LED1, 0);
PIN_setOutputValue(ledPinHandle, Board_LED2, 0);
rxTask_init(ledPinHandle); //original code
UartTask_init(); //add by WBJ
/* Start BIOS */
BIOS_start();
return (0);
}
在不同的task里面,使用event或者queue来实现消息传递就可以了
http://www.deyisupport.com/question_answer/wireless_connectivity/f/45/p/105583/285000.aspx#285000
贴了个我写的例程 供参考