This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC1310 15.4 sensor 怎么设置 RF发射 功率最大化 ,

Part Number: CC1310


CC1310  15.4  sensor   怎么设置 RF 功率最大化   

Predefined Symbols  CCFG_FORCE_VDDR_HH =1 设置后 程序报错  

RF 电压为1.67V   需要设置到 1.95V该怎么设置

  • 在433M设置CCFG_FORCE_VDDR_HH =1 后,必须将发射功率改为15dBm

    在config.h中做如下修改:

    #else
    #if ((CONFIG_PHY_ID == APIMAC_GENERIC_CHINA_433_PHY_128) || (CONFIG_PHY_ID == APIMAC_GENERIC_CHINA_LRM_433_PHY_130))
    #define CONFIG_TRANSMIT_POWER  15  //14

  • 设置成功  谢谢指导 

    实际上 在 15.4 sensor  里面  ccfg.c 无需设置

    1.Predefined Symbols  CCFG_FORCE_VDDR_HH =1 

    2.config.h    271行   

     #define CONFIG_TRANSMIT_POWER  15  //14

    3.  305行   

    /#error "CONFIG_TRANSMIT_POWER should be 14"

    4.右键项目--Predfined--Predefined Symbols  -Add..- Pre-define NAME...-CCFG_FORCE_VDDR_HH=1--Apply and Close

    4.成功测得 1.95V