CC1310 15.4 sensor 怎么设置 RF 功率最大化
Predefined Symbols CCFG_FORCE_VDDR_HH =1 设置后 程序报错
RF 电压为1.67V 需要设置到 1.95V该怎么设置
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
设置成功 谢谢指导
实际上 在 15.4 sensor 里面 ccfg.c 无需设置
1.Predefined Symbols CCFG_FORCE_VDDR_HH =1
2.config.h 271行
#define CONFIG_TRANSMIT_POWER 15 //14
3. 305行
/#error "CONFIG_TRANSMIT_POWER should be 14"
4.右键项目--Predfined--Predefined Symbols -Add..- Pre-define NAME...-CCFG_FORCE_VDDR_HH=1--Apply and Close
4.成功测得 1.95V