This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 不同频率下,WOR数据接收

Part Number: CC1310

目前正在开发一款设备X,使用CC1310作为无线传输模块。

设备X的WOR接收模式有两种,分别为模式A与模式B,二者的无线频率不同。

模式A的WOR接收周期为200ms,模式B的WOR接收周期为40ms。

设备X正常待机时,接收模式A和接收模式B二者交替执行。

如果有另一个设备Y,每隔10-15秒,采用与接收模式B相匹配的WOR发射模式发送无线数据。

请问有什么方法能保证设备X能够每次都接收到Y发送的数据呢?(设备Y不能长时间发送,需要满足1小时内,无线占空比小于1%,即发送总时间不得大于36秒)