This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 自己根据cc1310launchpad原理图自己画了一个板子,使用ccs通过launchpad跳线TMS TCK 3.3V GND R 无法下载程序

Part Number: CC1310

自己画的板子如图: ,通过将launchpad的下载接口(P4对应的跳线帽拿掉)接到自己板子上接了5个接口,分别为TMS-TMS R-nRESET TCK-TCK 3V3-V3.3 GND-GND。如图:

下载时提示错误:Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.6.0.00172)
Cortex_M3_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.6.0.00172)

x 出现错误。请重试或与管理员联系。