This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530外部晶振是否必须程序配置才能启动?

Other Parts Discussed in Thread: CC2530

请问刚出厂的CC2530芯片外接的32MHz晶振和32.768kHz晶振是不是都需要用户自己向芯片中烧写相应的配置程序才能启动?还是说新出厂的芯片只要上电后,首先自动启动RC16MHz晶振,然后芯片内部会自动由RC16MHz晶振跳转至32MHz外部晶振?

32MHz晶振和32.768kHz晶振起振前后的电压大概都是多少呢?

CC2530无法烧入程序和外部晶振起振与否相关吗?

非常期待您的回复!谢谢!

  • RC Oscillator 和 Crystal 的转换需要配置寄存器。晶振电平请测量TI参考设计板。

    The device has one internal system clock, or main clock. The source for the system clock can be either
    the 16-MHz RC oscillator or the 32-MHz crystal oscillator. Clock control is performed using the
    CLKCONCMD SFR register.

    请在TI网站下载查看文档:

    CC253x System-on-Chip Solution for 2.4-GHz IEEE 802.15.4 and ZigBee® Applications

    Literature Number: SWRU191C

    April 2009 – Revised January 2012