请问刚出厂的CC2530芯片外接的32MHz晶振和32.768kHz晶振是不是都需要用户自己向芯片中烧写相应的配置程序才能启动?还是说新出厂的芯片只要上电后,首先自动启动RC16MHz晶振,然后芯片内部会自动由RC16MHz晶振跳转至32MHz外部晶振?
32MHz晶振和32.768kHz晶振起振前后的电压大概都是多少呢?
CC2530无法烧入程序和外部晶振起振与否相关吗?
非常期待您的回复!谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问刚出厂的CC2530芯片外接的32MHz晶振和32.768kHz晶振是不是都需要用户自己向芯片中烧写相应的配置程序才能启动?还是说新出厂的芯片只要上电后,首先自动启动RC16MHz晶振,然后芯片内部会自动由RC16MHz晶振跳转至32MHz外部晶振?
32MHz晶振和32.768kHz晶振起振前后的电压大概都是多少呢?
CC2530无法烧入程序和外部晶振起振与否相关吗?
非常期待您的回复!谢谢!
RC Oscillator 和 Crystal 的转换需要配置寄存器。晶振电平请测量TI参考设计板。
The device has one internal system clock, or main clock. The source for the system clock can be either
the 16-MHz RC oscillator or the 32-MHz crystal oscillator. Clock control is performed using the
CLKCONCMD SFR register.
请在TI网站下载查看文档:
CC253x System-on-Chip Solution for 2.4-GHz IEEE 802.15.4 and ZigBee® Applications
Literature Number: SWRU191C
April 2009 – Revised January 2012