This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 运行一段时间后,电容出现漏电流大情况

Part Number: CC1310

采用电池供电(最大3.7V),用于温度测量,采用NTC温敏电阻。模块批量生产完测电流都是正常几个uA,一直运行一段时间后,再测电流,发现出现部分模块电流偏大,达到2~10mA,通过一一排查发现,有的是电源上的100nF异常,有的是电源上的22uF的电容异常,导致漏电流偏大;100nF的耐压为16V, 22uF的耐压为6.3V, 三星的电容。 会是什么原因会导致这种情况发生,有可能是板上的射频信号反射的能量累积损坏电容,还是其他什么原因;