This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101: PLL Lock Detector Output PLL lock detector output is not 100% reliable,怎么解决?

Part Number: CC1101


1.PLL LOCK 检测的方法,是否按照下述进行配置,就可以了?那如果是频繁检测到引脚的电平变化,接收几次数据就跳变,这个可能会是什么问题??

1.Program register IOCFGx.GDOx_CFG=0x0A and use the lock detector output available on the GDOx pin as an interrupt for the MCU. 

2.出现PLL LOCK  detector时候,怎么处理??

  • 1.是的

    2.检测是为了校准,在校准状态后将始终进入 TX 或 RX 状态

    数据手册22章介绍了PLL Lock Detector的一些详细的说明: https://www.ti.com.cn/cn/lit/ds/symlink/cc1101.pdf

    你遇到传输的具体问题是什么,数据传输失败还是其他的什么

  • 我的使用方式是两个CC1101会同步发送相同数据帧(433频段使用),另外会有多个CC1101处于接收状态,随时接收数据,但发现会出现数据会出现接收误码的情况,这个情况下设置了 IOCFGx.GDOx_CFG=0x0A,并在MCU中断检测该引脚的下降沿(默认PLL lock 是高电平变为低电平?)。分析其中接收的两个CC1101模块,发现其中一个在接收误码的时候,会伴随PLL lock 失效的情况。另外一个发现接收过程中无规律的出现PLL LOCK 反馈引脚高低频繁变化。那么,就想确认几个问题:1.只配置该寄存器,是否正确引出了检测反馈?2.出现电平频繁由高低反复切换情况,是否意味PLL LOCK确认失效又自动恢复?那么该失效情况下,误码接收是否会必然出现?3.校准是否每次出现时必要的操作??4.如果不进行校准,是否可以其他办法解决误码问题?

  • 有什么办法解决吗?

  • 并在MCU中断检测该引脚的下降沿(默认PLL lock 是高电平变为低电平?

    The lock detector output available on the GDOx pin should then be an interrupt for the MCU (x = 0,1, or 2). A positive transition on the GDOx pin means that the PLL is in lock.

    出现误码率高也有可能是硬件有问题,如果硬件有问题,配置了PLL误码率也不会改善,建议先用smartRF studio进行测试,以验证是否硬件有问题