This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 最小RX带宽

Part Number: CC1310

目前计算CC1310的最小RX带宽,在选型滤波器,

在CC13xx/CC26xx 硬件配置和 PCB 设计注意事项文件的12.5.2小节中 介绍了这个公式:

确保接收所需的最小 RX 带宽由下式给出: RX BW = Signal Bandwidth(信号带宽) + 4*ppm Crystal(晶体) * RF Frequency of Operation(运行频率) (7)

对于 FSK,信号带宽可以近似表示为数据速率 + 2*频率偏差(卡森法则)。
1.其中想请问CC1310在高速4M下的频率偏差是多少?

2.已知数据速率是4M,选用晶振的ppm值为10ppm,RF运行频率为868M
滤波器目前选择型号为:BALF-SPI-01D3

请问这款产品和CC1310频率偏移是否过大?或者推荐下更适合的滤波器。