This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: CC1310 如何修改通信模式?

Part Number: CC1310


我需要根据不同的空速修改不同的模式,如下图所示,例如我625空速使用的legacy long range模式,当我切换到5k空速时,我希望使用simplilink long range。

根据各空速生成的smartrf_settings.c文件进行文件对比,我将其中的不同参数已经了修改,但是发现修改后仍然无法通信,我需要知道生成的smartrf_settings.c里面的参数在我主函数哪一步之前调用的,以及如何才能进行参数修改以及切换。下图是修改的部分参数截图,以及在RF初始化之前进行的修改语句。

使用搜索功能,看不到smartrf_setting.c的参数赋值的位置。

  • 您好,

    感谢您的对TI产品的关注!为更加有效地解决您的问题,我需要多一些时间查看这款芯片,稍后会为您解答。

  • 您好,

    我不确定我是否理解您的问题和您给出的显示的数字。

    如果您想要同时使用传统 lrm (625 bps) 和 SimpleLink lrm (5 kbps),您需要在 smartrf_settings 文件中包含这两种模式的所有设置、覆盖、补丁:

    //*********************************************************************************
    // Parameter summary
    // RX Address0: 0xAA 
    // RX Address1: 0xBB 
    // RX Address Mode: No address check 
    // Frequency: 868.00000 MHz
    // Data Format: Serial mode disable 
    // Deviation: 5.000 kHz
    // Packet Length Config: Variable 
    // Max Packet Length: 255 
    // Packet Length: 20 
    // Packet Data: 255 
    // RX Filter BW: 39 kHz
    // Symbol Rate: 10.00061 kBaud
    // Sync Word Length: 32 Bits 
    // TX Power: 14 dBm (requires define CCFG_FORCE_VDDR_HH = 1 in ccfg.c, see CC13xx/CC26xx Technical Reference Manual)
    // Whitening: No whitening 
    
    #include "smartrf_settings.h"
    
    #include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_lrm.h)
    #include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_lrm.h)
    
    // TI-RTOS RF Mode Object
    RF_Mode RF_prop =
    {
        .rfMode = RF_MODE_PROPRIETARY_SUB_1,
        .cpePatchFxn = &rf_patch_cpe_lrm,
        .mcePatchFxn = 0,
        .rfePatchFxn = &rf_patch_rfe_lrm
    };
    
    
    // Overrides for CMD_PROP_RADIO_DIV_SETUP
    uint32_t pOverrides_625[] =
    {
        // override_use_patch_prop_lrm.xml
        // PHY: Use MCE ROM bank 3, RFE RAM patch
        MCE_RFE_OVERRIDE(0,3,0,1,0,0),
        // override_synth_prop_863_930_div5.xml
        // Synth: Set recommended RTRIM to 7
        .
        .
        .
        (uint32_t)0xFFFFFFFF
    };
    
    
    // CMD_PROP_RADIO_DIV_SETUP
    // Proprietary Mode Radio Setup Command for All Frequency Bands
    rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup_625 =
    {
        .commandNo = 0x3807,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
        .startTime = 0x00000000,
        .
        .
        .
        .pRegOverride = pOverrides_625,
        .centerFreq = 0x0364,
        .intFreq = 0x8000,
        .loDivider = 0x05
    };
    
    
    // CMD_FS
    // Frequency Synthesizer Programming Command
    rfc_CMD_FS_t RF_cmdFs_625 =
    {
        .commandNo = 0x0803,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
        .
        .
    };
    
    
    // CMD_PROP_TX
    // Proprietary Mode Transmit Command
    rfc_CMD_PROP_TX_t RF_cmdPropTx_625 =
    {
        .commandNo = 0x3801,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
       .
       .
       .
    };
    
    
    // CMD_PROP_RX
    // Proprietary Mode Receive Command
    rfc_CMD_PROP_RX_t RF_cmdPropRx_625 =
    {
        .commandNo = 0x3802,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
        .startTime = 0x00000000,
       .
       .
       .
    };
    
    
    //*********************************************************************************
    // Parameter summary
    // RX Address0: 0xAA 
    // RX Address1: 0xBB 
    // RX Address Mode: No address check 
    // Frequency: 868.00000 MHz
    // Data Format: Serial mode disable 
    // Deviation: 5.000 kHz
    // Packet Length Config: Variable 
    // Max Packet Length: 255 
    // Packet Length: 20 
    // Packet Data: 255 
    // RX Filter BW: 49 kHz
    // Symbol Rate: 19.99969 kBaud
    // Sync Word Length: 32 Bits 
    // TX Power: 14 dBm (requires define CCFG_FORCE_VDDR_HH = 1 in ccfg.c, see CC13xx/CC26xx Technical Reference Manual)
    // Whitening: CC1101/CC2500 compatible 
    
    #include "smartrf_settings.h"
    
    #include DeviceFamily_constructPath(rf_patches/rf_patch_cpe_sl_longrange.h)
    #include DeviceFamily_constructPath(rf_patches/rf_patch_rfe_sl_longrange.h)
    #include DeviceFamily_constructPath(rf_patches/rf_patch_mce_sl_longrange.h)
    
    // TI-RTOS RF Mode Object
    RF_Mode RF_prop =
    {
        .rfMode = RF_MODE_PROPRIETARY_SUB_1,
        .cpePatchFxn = &rf_patch_cpe_sl_longrange,
        .mcePatchFxn = &rf_patch_mce_sl_longrange,
        .rfePatchFxn = &rf_patch_rfe_sl_longrange
    };
    
    
    // Overrides for CMD_PROP_RADIO_DIV_SETUP
    uint32_t pOverrides_5k[] =
    {
        // override_use_patch_simplelink_long_range.xml
        // PHY: Use MCE RAM patch, RFE RAM patch
        MCE_RFE_OVERRIDE(1,0,0,1,0,0),
        // override_synth_prop_863_930_div5_lbw60k.xml
        // Synth: Set recommended RTRIM to 7
        HW_REG_OVERRIDE(0x4038,0x0037),
        .
        .
        .
        (uint32_t)0xFFFFFFFF
    };
    
    
    // CMD_PROP_RADIO_DIV_SETUP
    // Proprietary Mode Radio Setup Command for All Frequency Bands
    rfc_CMD_PROP_RADIO_DIV_SETUP_t RF_cmdPropRadioDivSetup_5k =
    {
        .commandNo = 0x3807,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
        .startTime = 0x00000000,
        .
        .
        .
        .pRegOverride = pOverrides_5k,
        .centerFreq = 0x0364,
        .intFreq = 0x8000,
        .loDivider = 0x05
    };
    
    
    // CMD_FS
    // Frequency Synthesizer Programming Command
    rfc_CMD_FS_t RF_cmdFs_5k =
    {
        .commandNo = 0x0803,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
        .startTime = 0x00000000,
        .startTrigger.triggerType = 0x0,
        .
        .
        .
    };
    
    
    // CMD_PROP_TX
    // Proprietary Mode Transmit Command
    rfc_CMD_PROP_TX_t RF_cmdPropTx_5k =
    {
        .commandNo = 0x3801,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
        .
        .
        .
    };
    
    
    // CMD_PROP_RX
    // Proprietary Mode Receive Command
    rfc_CMD_PROP_RX_t RF_cmdPropRx_5k =
    {
        .commandNo = 0x3802,
        .status = 0x0000,
        .pNextOp = 0, // INSERT APPLICABLE POINTER: (uint8_t*)&xxx
       .
       .
       .
    };

    在PHY间更改,您可以简单地用一个 PHY 打开 RF drive,做任何您想做的事情,然后关闭drive,然后用另一个 PHY 再次打开它。

    Smartrf Studio中导出的代码同时只会给你一个PHY,所以你首先要导出一个PHY,重命名它,然后导出另一个,并将设置粘贴到第一个的文件中(或者可以在代码中有两个不同的SmartRF_settings文件,不同的 PHY 具有不同的名称。