Other Parts Discussed in Thread: WI-SUN
请问TI Wi-SUN选择的通道功能是哪个?我这尝试和别家的Wi-SUN互联互通,结果边界路由发了PA帧就报错误状态码“100”,并且TI的demo中没找到100的状态码。
重点怀疑这个通道功能,“ Channel Function field ”。(注,能收到对方边界路由的PA帧).
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问TI Wi-SUN选择的通道功能是哪个?我这尝试和别家的Wi-SUN互联互通,结果边界路由发了PA帧就报错误状态码“100”,并且TI的demo中没找到100的状态码。
重点怀疑这个通道功能,“ Channel Function field ”。(注,能收到对方边界路由的PA帧).
SDK:simplelink_cc13xx_cc26xx_sdk_6_20_00_29
因为是跳频,所以没有抓到完整数据包。
PHY配置项如下:
Channel Function :Frequency Hopping
Based On RF Design:LP_CC1352P7-1
Region:EU
Regulatory Domain:0x03
Phy Mode ID: Mode 5, 150 Kbps, Mod Index 0.5
Operating Mode ID:3
Operating Mode Class:2
Channel Plan ID:33
Select a Custom Channel Plan:Null 未选择
一下为默认值自动生成
Center Frequency Channel 0 (MHz):863.1
Channel Spacing (kHz):200
Total Channels:35.