This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc1110 低功耗睡眠PM2 问题



大家好。
       原计发送广播信息一次后设置定时器参数再进入睡眠状态PM2,现在我通过uA表看到电流远不只文档上说的0.8uA。
       通过调试最后发现居然执行BSP_Init();后睡眠模式就不好使了(睡眠代码放到这行前确实为0.8uA)。

BSP_Init();   //假如注释这句就能去到0.9uA左右。
//Init_SLEEP_TIMER_5s();  
P1DIR = 0x03;  
while(1) PowerMode(2);

      这里测试永远都是100uA左右,请问无线发射后怎么进入PM2模式?

谢谢。

  • Hello George,

    BSP_Init()是不是把P1、P2口的状态改变了?
    可以试试将P1、P2口设置成下拉输入 (P2INT.PDUP2 and P2INT.PDUP1 = 1 ///  P2INP.MDP2[4:0] and P1INP.MDP1_[7:2] = 0).

     PowerMode(2)不就是进入PM2模式的函数吗?

  • 你好Martin。确实类似是这样,谢谢。P0INP = 0; 这样就可以了。
    但遇到一个问题是,我现在在不加底板(外围设备)确实是0.9uA了。

    1.我想问问如何关闭cc1110 对外供电?因为我接的一个学习底座板(XWWK-CC1110-02(RS232))好像默认是常闭电路,而且还拖个LED。
    2.假如无法关闭(不能取消对外供电——就算在PM2下),这样我连接其他传感器或者常闭的电路,那不就很耗电?

  • Hi George,

    CC1110对外供电?不太明白你具体指的是什么?能详细说明一下你用的是哪个pin,设置的是哪个寄存器吗?

    如果你连接传感器,可以考虑增加一个电源管理的芯片,在CC1110进入PM2之前通过那个电源管理芯片将传感器的电源关闭。

  • 你好Martin.
           谢谢你的回答,我已经在另外一个贴开了新的提问了。