Other Parts Discussed in Thread: MPY634
MPY634倍频电路如下,照这图用万用板焊了的电路,频率是倍上去了,但输出波形式一高一低的正弦波,输出波形如图片所示。这问题怎么解决??谢谢!!
测试图片
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
手册上面有这么一段,不知道是针对芯片内部而言还是管脚SF的电压值就对应这个比例值(即10V代表1/10,但从手册上来看应该就是SF脚的电压值)。手册部分内容如下
The scale factor is accurately factory adjusted to 10V and is
typically accurate to within 0.1% or less. The scale factor
may be adjusted by connecting a resistor or potentiometer
between pin SF and the –VS power supply.
SF PIN我也测过了 如果按照正负15V供电 其电位约在-14V左右
但这应该不是IC本身的问题 最粗略的 您可以搭建LZ的电路 输入共模范围内的直流电压
然后直接测量Vout 看看是否符合运算式 也可以按照手册添加电阻改变增益
至少我的结果完全符合手册
您看一下http://www.ti.com.cn/cn/lit/an/sbfa006/sbfa006.pdf这个应用手册 里面有此IC的框图
带隙和GND并无直接关系 所谓10V的参考点也很可能不是GND
不论如何 根据结果来看 Ref向内部提供的电压是无误的 我拿到的样片也不是次品
BTW:正规渠道的次品......反正我是没中过彩;TI的手册我也看岔过,基本都是我自己nc
这颗是 Analog 的料,到这个版块讨论不是很对口啊!建议到对应版面,这样得到的关注度会更高。