This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1120的问题,麻烦解答下

Other Parts Discussed in Thread: CC1120, CC1101

最近在调CC1120。

CC1120初始寄存器遇到的设置问题: 
1.通过Smart RFStudio设置生成的一些寄存器值,放到代码里面不能正常通信。在433Mhz, 1200bps情况下Smart RFStudio设置生成的值为:
// Rf settings for CC1120
RF_SETTINGS code rfSettings = {
    0xB0,  // IOCFG3              GPIO3 IO Pin Configuration
    0x06,  // IOCFG2              GPIO2 IO Pin Configuration
    0xB0,  // IOCFG1              GPIO1 IO Pin Configuration
    0x40,  // IOCFG0              GPIO0 IO Pin Configuration
    0x0B,  // SYNC_CFG1           Sync Word Detection Configuration
    0x1C,  // DCFILT_CFG          Digital DC Removal Configuration
    0x18,  // PREAMBLE_CFG1       Preamble Length Configuration
    0xC6,  // IQIC                Digital Image Channel Compensation Configuration
    0x08,  // CHAN_BW             Channel Filter Configuration
    0x05,  // MDMCFG0             General Modem Parameter Configuration
    0x20,  // AGC_REF             AGC Reference Level Configuration
    0x19,  // AGC_CS_THR          Carrier Sense Threshold Configuration
    0xA9,  // AGC_CFG1            AGC Configuration
    0xCF,  // AGC_CFG0            AGC Configuration
    0x00,  // FIFO_CFG            FIFO Configuration
    0x03,  // SETTLING_CFG        Frequency Synthesizer Calibration and Settling Configuration
    0x14,  // FS_CFG              Frequency Synthesizer Configuration
    0x20,  // PKT_CFG0            Packet Configuration, Reg 0
    0xFF,  // PKT_LEN             Packet Length Configuration
    0x00,  // IF_MIX_CFG          IF Mix Configuration
    0x22,  // FREQOFF_CFG         Frequency Offset Correction Configuration
    0x6C,  // FREQ2               Frequency Configuration [23:16]
    0x80,  // FREQ1               Frequency Configuration [15:8]
    0x00,  // FS_DIG1             
    0x5F,  // FS_DIG0             
    0x40,  // FS_CAL1             
    0x0E,  // FS_CAL0             
    0x03,  // FS_DIVTWO           Divide by 2
    0x33,  // FS_DSM0             Digital Synthesizer Module Configuration, Reg 0
    0x17,  // FS_DVC0             Divider Chain Configuration, Reg 0
    0x50,  // FS_PFD              Phase Frequency Detector Configuration
    0x6E,  // FS_PRE              Prescaler Configuration
    0x14,  // FS_REG_DIV_CML      
    0xAC,  // FS_SPARE            
    0xB4,  // FS_VCO0             VCO Configuration, Reg 0
    0x0E,  // XOSC5               Crystal Oscillator Configuration, Reg 5
    0x03,  // XOSC1               Crystal Oscillator Configuration, Reg 1
};
 
2.下载官网的demo程序(CC1120 software_swrc219)看了下,多了几个关键寄存器,拷贝到我代码里,目前能正常通信但是之前  CC1101等调试都是以Smart RFStudio生成的寄存器配置为准,不知道此份设置是否稳定?
 
官方的例程设置如下:
// Modem settings for test case 1 adjusted to 25kHz RXBW and 4 Byte preamble(")*/ CC1120工程中
const registerSetting_t cc112xLowDataRateRfSettings[] =  
{
  {CC112X_IOCFG0            ,0x06}, // Route sync signal to GPIO0
  {CC112X_FS_DIG1           ,0x00},
  {CC112X_FS_DIG0           ,0x5F},
  {CC112X_FS_CAL0           ,0x0E},
  {CC112X_FS_DIVTWO         ,0x03},
  {CC112X_FS_DSM0           ,0x33},
  {CC112X_FS_DVC0           ,0x17},  
  {CC112X_FS_PFD            ,0x50},  
  {CC112X_FS_PRE            ,0x6E},
  {CC112X_FS_REG_DIV_CML    ,0x14},
  {CC112X_FS_SPARE          ,0xAC},
  {CC112X_XOSC5             ,0x0E},
  {CC112X_XOSC4             ,0xA0},
  {CC112X_XOSC3             ,0xC7},  
  {CC112X_XOSC1             ,0x03},
  {CC112X_ANALOG_SPARE      ,0x00},
  {CC112X_FIFO_CFG          ,0x00},
  {CC112X_DEV_ADDR          ,0x00},  
  {CC112X_SETTLING_CFG      ,0x0B},
  {CC112X_FS_CFG            ,0x12}, //////////////////////////////////////////////////////////////////
  {CC112X_PKT_CFG2          ,0x00},
  {CC112X_PKT_CFG1          ,0x05}, // Address check off and CRC check on
  {CC112X_PKT_CFG0          ,0x20},  
  {CC112X_RFEND_CFG1        ,0x0F}, // Stay in RX after RX, No timeout for sync word search  
  {CC112X_RFEND_CFG0        ,0x00}, // IDle after TX, no interferring from MARC  
  {CC112X_SYNC3             ,0x93},/////////////////////////////////////////////////////////////////////
  {CC112X_SYNC2             ,0x0B}, 
  {CC112X_SYNC1             ,0x51}, 
  {CC112X_SYNC0             ,0xDE}, 
  {CC112X_SYNC_CFG1         ,0x0B}, 
  {CC112X_SYNC_CFG0         ,0x17}, 
  {CC112X_DEVIATION_M       ,0x06}, // (4000 Hz)       
  {CC112X_MODCFG_DEV_E      ,0x03}, // (4000 Hz)       
  {CC112X_DCFILT_CFG        ,0x1C}, //                 
  {CC112X_PREAMBLE_CFG1     ,0x18}, // 4" byte preamble 
  {CC112X_PREAMBLE_CFG0     ,0x2A}, //                 
  {CC112X_FREQ_IF_CFG       ,0x40}, // (62500 Hz)      
  {CC112X_IQIC              ,0xC6}, //                 
  {CC112X_CHAN_BW           ,0x08}, // (25000" Hz)      
  {CC112X_MDMCFG1           ,0x46}, //                 
  {CC112X_MDMCFG0           ,0x05}, //                 
  {CC112X_DRATE2            ,0x43}, // (1200 bps)      
  {CC112X_DRATE1            ,0xA9}, // (1200 bps)      
  {CC112X_DRATE0            ,0x2A}, // (1200 bps)      
  {CC112X_AGC_REF           ,0x20}, 
  {CC112X_AGC_CS_THR        ,0x19}, 
  {CC112X_AGC_GAIN_ADJUST   ,0x00}, 
  {CC112X_AGC_CFG3          ,0x91}, 
  {CC112X_AGC_CFG2          ,0x20}, 
  {CC112X_AGC_CFG1          ,0xA9}, 
  {CC112X_AGC_CFG0          ,0xCF}, 
  {CC112X_PA_CFG2           ,0x7F}, 
  {CC112X_PA_CFG1           ,0x56}, 
  {CC112X_PA_CFG0           ,0x7C}, 
  {CC112X_IF_MIX_CFG        ,0x00}, 
  {CC112X_FREQOFF_CFG       ,0x22}, 
  {CC112X_TOC_CFG           ,0x0B},
  {CC112X_SOFT_TX_DATA_CFG  ,0x00}
};
 
 
3.此次调试RSSI值有误(是按照CC1101的RSSI的那套代码)不知道1120的RSSI跟之前的1101是否有大的变动?CC1120跟之前的系列低功耗方面是否也有大的变动?
 
麻烦Ti的工程师解决下疑问?