最近在调CC1120。
CC1120初始寄存器遇到的设置问题:1.通过Smart RFStudio设置生成的一些寄存器值,放到代码里面不能正常通信。在433Mhz, 1200bps情况下Smart RFStudio设置生成的值为:// Rf settings for CC1120RF_SETTINGS code rfSettings = {0xB0, // IOCFG3 GPIO3 IO Pin Configuration0x06, // IOCFG2 GPIO2 IO Pin Configuration0xB0, // IOCFG1 GPIO1 IO Pin Configuration0x40, // IOCFG0 GPIO0 IO Pin Configuration0x0B, // SYNC_CFG1 Sync Word Detection Configuration0x1C, // DCFILT_CFG Digital DC Removal Configuration0x18, // PREAMBLE_CFG1 Preamble Length Configuration0xC6, // IQIC Digital Image Channel Compensation Configuration0x08, // CHAN_BW Channel Filter Configuration0x05, // MDMCFG0 General Modem Parameter Configuration0x20, // AGC_REF AGC Reference Level Configuration0x19, // AGC_CS_THR Carrier Sense Threshold Configuration0xA9, // AGC_CFG1 AGC Configuration0xCF, // AGC_CFG0 AGC Configuration0x00, // FIFO_CFG FIFO Configuration0x03, // SETTLING_CFG Frequency Synthesizer Calibration and Settling Configuration0x14, // FS_CFG Frequency Synthesizer Configuration0x20, // PKT_CFG0 Packet Configuration, Reg 00xFF, // PKT_LEN Packet Length Configuration0x00, // IF_MIX_CFG IF Mix Configuration0x22, // FREQOFF_CFG Frequency Offset Correction Configuration0x6C, // FREQ2 Frequency Configuration [23:16]0x80, // FREQ1 Frequency Configuration [15:8]0x00, // FS_DIG10x5F, // FS_DIG00x40, // FS_CAL10x0E, // FS_CAL00x03, // FS_DIVTWO Divide by 20x33, // FS_DSM0 Digital Synthesizer Module Configuration, Reg 00x17, // FS_DVC0 Divider Chain Configuration, Reg 00x50, // FS_PFD Phase Frequency Detector Configuration0x6E, // FS_PRE Prescaler Configuration0x14, // FS_REG_DIV_CML0xAC, // FS_SPARE0xB4, // FS_VCO0 VCO Configuration, Reg 00x0E, // XOSC5 Crystal Oscillator Configuration, Reg 50x03, // XOSC1 Crystal Oscillator Configuration, Reg 1};2.下载官网的demo程序(CC1120 software_swrc219)看了下,多了几个关键寄存器,拷贝到我代码里,目前能正常通信,但是之前 CC1101等调试都是以Smart RFStudio生成的寄存器配置为准,不知道此份设置是否稳定?官方的例程设置如下:// Modem settings for test case 1 adjusted to 25kHz RXBW and 4 Byte preamble(")*/ CC1120工程中const registerSetting_t cc112xLowDataRateRfSettings[] ={{CC112X_IOCFG0 ,0x06}, // Route sync signal to GPIO0{CC112X_FS_DIG1 ,0x00},{CC112X_FS_DIG0 ,0x5F},{CC112X_FS_CAL0 ,0x0E},{CC112X_FS_DIVTWO ,0x03},{CC112X_FS_DSM0 ,0x33},{CC112X_FS_DVC0 ,0x17},{CC112X_FS_PFD ,0x50},{CC112X_FS_PRE ,0x6E},{CC112X_FS_REG_DIV_CML ,0x14},{CC112X_FS_SPARE ,0xAC},{CC112X_XOSC5 ,0x0E},{CC112X_XOSC4 ,0xA0},{CC112X_XOSC3 ,0xC7},{CC112X_XOSC1 ,0x03},{CC112X_ANALOG_SPARE ,0x00},{CC112X_FIFO_CFG ,0x00},{CC112X_DEV_ADDR ,0x00},{CC112X_SETTLING_CFG ,0x0B},{CC112X_FS_CFG ,0x12}, //////////////////////////////////////////////////////////////////{CC112X_PKT_CFG2 ,0x00},{CC112X_PKT_CFG1 ,0x05}, // Address check off and CRC check on{CC112X_PKT_CFG0 ,0x20},{CC112X_RFEND_CFG1 ,0x0F}, // Stay in RX after RX, No timeout for sync word search{CC112X_RFEND_CFG0 ,0x00}, // IDle after TX, no interferring from MARC{CC112X_SYNC3 ,0x93},/////////////////////////////////////////////////////////////////////{CC112X_SYNC2 ,0x0B},{CC112X_SYNC1 ,0x51},{CC112X_SYNC0 ,0xDE},{CC112X_SYNC_CFG1 ,0x0B},{CC112X_SYNC_CFG0 ,0x17},{CC112X_DEVIATION_M ,0x06}, // (4000 Hz){CC112X_MODCFG_DEV_E ,0x03}, // (4000 Hz){CC112X_DCFILT_CFG ,0x1C}, //{CC112X_PREAMBLE_CFG1 ,0x18}, // 4" byte preamble{CC112X_PREAMBLE_CFG0 ,0x2A}, //{CC112X_FREQ_IF_CFG ,0x40}, // (62500 Hz){CC112X_IQIC ,0xC6}, //{CC112X_CHAN_BW ,0x08}, // (25000" Hz){CC112X_MDMCFG1 ,0x46}, //{CC112X_MDMCFG0 ,0x05}, //{CC112X_DRATE2 ,0x43}, // (1200 bps){CC112X_DRATE1 ,0xA9}, // (1200 bps){CC112X_DRATE0 ,0x2A}, // (1200 bps){CC112X_AGC_REF ,0x20},{CC112X_AGC_CS_THR ,0x19},{CC112X_AGC_GAIN_ADJUST ,0x00},{CC112X_AGC_CFG3 ,0x91},{CC112X_AGC_CFG2 ,0x20},{CC112X_AGC_CFG1 ,0xA9},{CC112X_AGC_CFG0 ,0xCF},{CC112X_PA_CFG2 ,0x7F},{CC112X_PA_CFG1 ,0x56},{CC112X_PA_CFG0 ,0x7C},{CC112X_IF_MIX_CFG ,0x00},{CC112X_FREQOFF_CFG ,0x22},{CC112X_TOC_CFG ,0x0B},{CC112X_SOFT_TX_DATA_CFG ,0x00}};3.此次调试RSSI值有误(是按照CC1101的RSSI的那套代码)不知道1120的RSSI跟之前的1101是否有大的变动?CC1120跟之前的系列低功耗方面是否也有大的变动?麻烦Ti的工程师解决下疑问?