Part Number: LAUNCHXL-CC1310
在SmartRF Studio 7只有这两个频段,其他频段支持吗?怎么配置?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,CC13010支持以下三个频段
1.433MHz ISM频段
2.868MHz SRD频段
3.915MHz ISM频段
国内目前只支持433MHz,相关的问题我的同事已经对您进行回复了。
例程中有868MHz的配置,您上一个问题的回复链接链接中有更改成433MHz的配置。
在章节5.5中您可以查阅相关资料
希望能对您有所帮助