1.由于 产品要求支持4-fsk调制解调,芯片的datasheet显示可以支持,但根据给的案例和应用发现只有2-(G)FSK,没有4-FSK的应用,该怎么配置可以让芯片支持4-FSK的调制和解调。
2. 根据demo板的设计,输出是差分再经过LC转换为单端,差分阻抗在403M和413M是多少,是否可以复用433MHz的差分转单端设计,或者直接用巴伦转换的话,差分阻抗用100欧姆的可以吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
从 LAUNCH-CC433P-1352 设计中复制 4 MHz 部分:https://www.ti.com/lit/zip/swrc352
这将在 403 MHz 和 433 MHz 下很好地工作。
对于问题的 4-FSK 部分:e2e.ti.com/.../cc1312r-4-fsk-modulation-support