This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: OAD coprocessor 射频问题

Part Number: CC1312R

TI大神好:

1312 OAD例程

使用一个1312做coprocessor ,在linux 上启动collector,这样sensor节点无法连接到collector上.无法做OAD

我怀疑是射频配置问题,因为我是将1352生成的433射频配置同步到sensor和collector上,参考上一个帖子:

那么用1312做coprocessor 的时候是否需要修改射频参数?应该如何修改?我尝试了用1352的coprocessor ,但是这个例程中似乎无法配置433

SDK版本:simplelink_cc13xx_cc26xx_sdk_7_10_02_23

linux版本:ti154stack_linux_x64_4_40_00_03

另外,我尝试使用一块1310作为coprocessor 来测试OAD例程,这种情况下sensor是可以连接上来的,但是发送OAD命令(使用V命令),sensor没有响应.

麻烦确认一下,谢谢