Part Number: LAUNCHXL-CC1310
Other Parts Discussed in Thread: CC1310, UNIFLASH
我用的官方的例程 编译后 用XDS110无法下载 是需要配置吗? 报错如下图

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Board Reset Complete.
Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
Cortex_M3_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
Cortex_M3_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
Cortex_M3_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
板子的连线图应该没有问题 因为我用Flash Programmer 2 是可以下载HEX文件
一、抛开我自己的板子 我用买的官方CC1310 LanchPAD开发板 在线下载 程序是运行正常
二、同样的程序 我用CCS生产HEX文件 然后再用Flash Programmer 2下载后 程序也无法运行
三、我用的程序是官方提供的adcbufcontinuous_CC1310_LAUNCHXL_tirtos_ccs。
那么现在问题是 是不是我在CCS生产的HEX文件方法不对? 以下我贴出CCS配置输出HEX的贴图
下载完成后 信息提示>Initiate access to target: XDS-L2000L76 using 2-pin cJTAG.
>Reading file: D:/cc1210hjb/adcbufcontinuous_CC1310_LAUNCHXL_tirtos_ccs/Debug/adcbufcontinuous_CC1310_LAUNCHXL_tirtos_ccs.hex.
>Start flash erase ...
>Erase finished successfully.
>Start flash programming ...
>Programming finished successfully.
>Reset target ...
>Reset of target successful.
这里看应该是下载程序成功了 然后就是程序不运行,是不是烧写的方式不对 有个MULTIPE烧写方式 要选择那些文件
又搞了一个晚上 开发板现在用Flash Programmer 2 正常了 要下载.out文件 不能选择.hex文件
现在问题就聚焦在我自己设计的PCB板子 Flash Programmer 2可以下载out文件 但不运行 CCS不能下载程序
提示这个 有经验的帮忙分析一下
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Board Reset Complete.
Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
Cortex_M3_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
Cortex_M3_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
Cortex_M3_0: Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
Cortex_M3_0: Trouble Halting Target CPU: (Error -2064 @ 0x0) Unable to read device status. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.13.0.00201)
你先别对这个板子进行其他操作了,容易锁板
首先,你尝试复位
这种hex文件不能执行可能和编译器的有关,先看下复位后是否可以执行程序
然后,
您是否尝试使用 AJSM 模块?
据我所知,这是禁用对 DAP 访问的唯一方法。
如果 AJSM 中的默认密钥发生更改,则设备将被锁定(从调试访问的角度来看)。
只有当新的编程密钥已知时,才有办法解锁调试访问。
注意:必须使用特定实用程序来提供此新密钥,并且必须在每次开机重置时执行此操作。
看起来像是硬件方面的问题,做一个硬件审核
请问你复位后是否起作用?
关于锁定,你可以擦除芯片,和你之前的步骤一样,使用uniflash进行erase flash,这样可以解锁
nrst引脚直接加了一个10K的上拉电阻 接到下载口的rst引脚
这个没问题
让晶振起作用,看一下这个
https://e2echina.ti.com/support/wireless-connectivity/sub-1-ghz/f/sub-1-ghz-forum/190444/cc1310
外部高频晶振主要作用是为Radio信号提供时钟源
低频的32.768K的时钟主要用于设备休眠时钟,没有32.768K的低频晶振时程序会自动切换到内部低频RC