This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi 这几天在研究CC3200的电源管理方案,从数据手册和TRM手册以及CC3200-Power_Management_Framework中进行测试总结,整理的一份测试报告,测试数据和参考手册给出的略有差别,但量级大体相当,详细的测试笔记见附件,测试程序为idle_profile_nonos对程序稍加修改就可以测试CC3200的功耗,简单总结如下:
模式 |
条件 |
电流消耗 |
测试图 |
Datasheet |
M4 Active+NWP connect AP |
1 |
15.9mA |
图1 |
15.3mA |
M4 LPDS+NWP start but do nothing |
2 |
282uA |
图2 |
266uA |
M4 LPDS+NWP connect AP |
3 |
600uA~2mA |
图3 图4 |
825uA |
M4 LPDS+NWP Hib |
4 |
229uA |
图5 |
120uA |
M4 Hib+NWP Hib |
5 |
10.65uA |
图6 |
4uA |
你好,注意CC3200进入低功耗时,外围的SPI Flash也要进入低功耗模式,需要发指令给SPI Flash,还有就是外围的上拉电阻,下拉电阻不要太小,以免出现消耗电流的现象。
我记得在程序中进入低功耗模式时已经对CC3200的引脚进行处理,并且TI官方的Launchpad上也是很多管脚直接悬空的,还是建议多与TI的官方Demo板进行硬件对比,会不会在一些电感不同时有一定的能耗?