This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi 这几天在研究CC3200的电源管理方案,从数据手册和TRM手册以及CC3200-Power_Management_Framework中进行测试总结,整理的一份测试报告,测试数据和参考手册给出的略有差别,但量级大体相当,详细的测试笔记见附件,测试程序为idle_profile_nonos对程序稍加修改就可以测试CC3200的功耗,简单总结如下:
模式 |
条件 |
电流消耗 |
测试图 |
Datasheet |
M4 Active+NWP connect AP |
1 |
15.9mA |
图1 |
15.3mA |
M4 LPDS+NWP start but do nothing |
2 |
282uA |
图2 |
266uA |
M4 LPDS+NWP connect AP |
3 |
600uA~2mA |
图3 图4 |
825uA |
M4 LPDS+NWP Hib |
4 |
229uA |
图5 |
120uA |
M4 Hib+NWP Hib |
5 |
10.65uA |
图6 |
4uA |
注意程序开始的全局变量定义,用于不同模式的功耗测试
unsigned char APconnect=1; //测试sl_start 后 连接AP和不连接AP的功耗
unsigned char LPDS=1; //LPDS模式测试
你还,请教个问题,条件1的测试结果是连接到AP,没有进行数据收发得到的吗?如果有数据收或者发,功耗测试结果有吗?谢谢!