This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

大神们一起来讨论下:CC3200上打算接摄像头、SD卡、WIFI也必须用,这样会产生引脚冲突怎么解决?

Other Parts Discussed in Thread: CC3200, TIDC-CC3200-VIDEO

C3200上接摄像头,再接SD卡的话,采用SDHost方式时CMD(pXCLK)引脚冲突了;如果采用SPI模块方式,MOSI引脚就冲突,要么占用了32.768的时钟引脚,要么占用摄像头的pDATA10。大神们来讨论下,谢谢!

  • 你是用SD卡存摄像头的视频吗?

    http://www.docin.com/p-1436354793.html

    看这个参考,两者不冲突。

  • 谢谢!是安排存储些图片或者视频的。

    SD_SMD和Camera_pXCLK共用硬件引脚,软件使用时不影响就好。

  • 可以参考http://www.ti.com/tool/TIDC-CC3200CAMBOOST 有详细的设计文件

  • 你好,想问个问题,对于接sensor有点迷糊,CC3200是直接连OV3660的吗?还是中间要接ISP处理芯片的?还有这个功耗能做到多少?

  • 参考最新的TI 设计 SimpleLink™ CC3200-OV788 Video/Audio Streaming Over Wi-Fi Reference Design

    http://www.ti.com/tool/TIDC-CC3200-VIDEO

    Description

    The design enables OV788 ultra-low power video compression chip users to bring live streaming capabilities of audio and video data over Wi-Fi® very easily. It showcases a single chip implementation of RTP video streaming + Wi-Fi connection on the SimpleLink™ CC3200 Wi-Fi wireless micro-controller over 802.11 b/g/n networks from any smart phone, tablet, or computer over local network. This design implementation is well suited with a wide range of Internet of Things (IoT) applications such as battery operated intrusion cameras, door locks, video doorbells and 360-degree multi-cameras in smart homes taking advantage of easy commissioning to a Wi-Fi network and advanced low-power modes from the CC3200 Internet-on-a-chip™ solution.

    Features
    • Supports Capture and streaming of: Video - 720p @ 15FPS
    • Supports Capture and streaming of: Audio – PCM, 16bps @ 11025Hz
    • Supports RTP/RTSP protocols
    • SimpleLink™ Wi-Fi solution over 802.11 b/g/n networks
    Features • Supports capture and streaming of: – Video – 720p at 15FPS – Audio – PCM, 16 bps at 11025 Hz • Supports RTP/RTSP protocols – Compatible with media players supporting these protocols • SimpleLink™ Wi-Fi connectivity over 802.11 b/g/n networks from any smart phone, tablet, or computer over local network • Built-in provisioning for easy commissioning of the device to a Wi-Fi network • Advanced low-power modes Applications • Wireless Video Doorbells • Home and Baby Monitoring • Remote Surveillance • Wireless Announcement Systems