C3200上接摄像头,再接SD卡的话,采用SDHost方式时CMD(pXCLK)引脚冲突了;如果采用SPI模块方式,MOSI引脚就冲突,要么占用了32.768的时钟引脚,要么占用摄像头的pDATA10。大神们来讨论下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
C3200上接摄像头,再接SD卡的话,采用SDHost方式时CMD(pXCLK)引脚冲突了;如果采用SPI模块方式,MOSI引脚就冲突,要么占用了32.768的时钟引脚,要么占用摄像头的pDATA10。大神们来讨论下,谢谢!
参考最新的TI 设计 SimpleLink™ CC3200-OV788 Video/Audio Streaming Over Wi-Fi Reference Design
http://www.ti.com/tool/TIDC-CC3200-VIDEO
The design enables OV788 ultra-low power video compression chip users to bring live streaming capabilities of audio and video data over Wi-Fi® very easily. It showcases a single chip implementation of RTP video streaming + Wi-Fi connection on the SimpleLink™ CC3200 Wi-Fi wireless micro-controller over 802.11 b/g/n networks from any smart phone, tablet, or computer over local network. This design implementation is well suited with a wide range of Internet of Things (IoT) applications such as battery operated intrusion cameras, door locks, video doorbells and 360-degree multi-cameras in smart homes taking advantage of easy commissioning to a Wi-Fi network and advanced low-power modes from the CC3200 Internet-on-a-chip™ solution.