This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200的下载方式问题

Other Parts Discussed in Thread: UNIFLASH, CC3200

  • 新手求教,刚买了一个CC3200开发板(还没到手上),我先看了一下板子的说明文档,有几个地方不太明白:1、这个板子好像是可以通过芯片把USB配制成JTAG和UART的下载模式,对吧?  2、这里的JTAG和UART下载有何不同,说明手册SOP[2:0] = 000  是(Functional mode + 4 Wire JTAG),SOP[2:0] = 100 是Flash programming,那么这个Functional mode是不是就是仿真调试模式,能不能下载程序到flash中去?(或者这里的JTAG模式支持下载程序到flash里去么?),另外这个Flash programming说的就是通过UART方式下载进去flash么?如果是的话,通过UART下载程序到flash的方式支持在线仿真么? 3、uniflash工具往flash下载程序是利用UART还是JTAG的方式?下载完了可以CCS在线调试么?        问了好多,就是因为没彻底看懂文档说明,CC3200的开发板还没邮到我手里,麻烦那位大神能不能给新手答疑一下,非常感谢。