This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC3200 在存在 外设摄像头 时的 HIB唤醒方案

Other Parts Discussed in Thread: CC3200

1、使用芯片型号:CC3200 SimpleLink™ Wi-Fi®

2、外设:MT9D111摄像头、音频codecTLV320AIC3254、PMU和其它 外设

3、问题:在使用MT9D111摄像头条件下,怎么实现从LPDS或HIB唤醒

问题详述:在LPDS和HIB休眠模式下,只有下面这些IO可以唤醒MCU:

GPIO_02 57
GPIO_04 59
GPIO_11 2
GPIO_13 4
GPIO_17 8
GPIO_24 17

但这些IO中,pin 2、4、8、59被外设camera接口占用,pin17被I2C占用、pin57用于红外唤醒,现在需要另外一IO用于按键唤醒(考虑红外唤醒失效的情况下使用),但能唤醒的IO大部分被摄像头外设占用,无法实现在LPDS和HIB休眠模式下唤醒,请问有无解决方案?

  谢谢!