大家说用套接字测试还是用 AP模式啊? 麻烦大家指导一下,代码不会写》》》》
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,关于TCP数据传输的一些测试资料
|
Component |
Details |
|
Reference Host Platform |
CC3200, MSP430F5529 and SimpleLink Studio for Windows, |
|
Chip HW Version |
PG1.33R, CC3100, CC3200 |
|
HW platform |
Booster Pack Rev-3.2, Pack Rev-4.1 |
|
Host Version |
1.0.0.10 |
|
Build Version |
2.4.0.2.31.1.3.0.1.1.0.3.34 |
|
AP Mode |
|||
|
|
SL Studio |
CC3200 |
|
|
Security |
Traffic |
SPI 15MHz |
SPI 20MHz |
|
Open |
UDP Tx |
12.9Mbps |
16.0Mbps |
|
UDP Rx |
10.5Mbps |
16.1Mbps |
|
|
TCP Tx |
12.9Mbps |
16.4Mbps |
|
|
TCP Rx |
11.3Mbps |
15.1Mbps |
|
|
TLS |
TCP Tx |
12.5Mbps |
12.0Mbps |
|
TCP Rx |
11.3Mbps |
11.6Mbps |
|
|
SSL |
TCP Tx |
8.4Mbps |
8.1Mbps |
|
TCP Rx |
9.6Mbps |
9.9Mbps |
|
|
STA Mode |
|||
|
|
SL Studio |
CC3200 |
|
|
Security |
Traffic |
SPI 15MHz |
SPI 20MHz |
|
Open |
UDP Tx |
12.7Mbps |
15.9Mbps |
|
UDP Rx |
10.5Mbps |
16.1Mbps |
|
|
TCP Tx |
12.8Mbps |
16.2Mbps |
|
|
TCP Rx |
11.3Mbps |
15.3Mbps |
|
|
TLS |
TCP Tx |
12.8Mbps |
12.4Mbps |
|
TCP Rx |
11.1Mbps |
11.8Mbps |
|
|
SSL |
TCP Tx |
8.8Mbps |
8.5Mbps |
|
TCP Rx |
9.8Mbps |
9.8 Mbps |
|