This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI CC3200 TCP传输速率测试

Other Parts Discussed in Thread: MSP430F5529, CC3200, CC3100

大家说用套接字测试还是用 AP模式啊?  麻烦大家指导一下,代码不会写》》》》

  • 可以参考这边的socket例程: http://processors.wiki.ti.com/index.php/CC32xx_TCP_Socket_Application

  • 但是我们这有讲解怎么测TCP传输速率的资料吗?谢谢  

  • 你好,关于TCP数据传输的一些测试资料

    Component

    Details

    Reference Host Platform

    CC3200, MSP430F5529 and SimpleLink Studio for Windows,

    Chip HW Version

    PG1.33R, CC3100, CC3200

    HW platform

    Booster Pack Rev-3.2, Pack Rev-4.1

    Host Version

    1.0.0.10

    Build Version

    2.4.0.2.31.1.3.0.1.1.0.3.34

    AP Mode

     

    SL Studio

    CC3200

    Security

    Traffic

    SPI 15MHz
    Windows 7

    SPI 20MHz
    M4 80MHz

    Open

    UDP Tx

    12.9Mbps

    16.0Mbps

    UDP Rx

    10.5Mbps

    16.1Mbps

    TCP Tx

    12.9Mbps

    16.4Mbps

    TCP Rx

    11.3Mbps

    15.1Mbps

    TLS

    TCP Tx

    12.5Mbps

     12.0Mbps

    TCP Rx

    11.3Mbps

     11.6Mbps

    SSL

    TCP Tx

    8.4Mbps

     8.1Mbps

    TCP Rx

    9.6Mbps

     9.9Mbps

    STA Mode

     

    SL Studio

    CC3200

    Security

    Traffic

    SPI 15MHz
    Windows 7

    SPI 20MHz
    M4 80MHz

    Open

    UDP Tx

    12.7Mbps

    15.9Mbps

    UDP Rx

    10.5Mbps

    16.1Mbps

    TCP Tx

    12.8Mbps

    16.2Mbps

    TCP Rx

    11.3Mbps

    15.3Mbps

    TLS

    TCP Tx

    12.8Mbps

    12.4Mbps

    TCP Rx

    11.1Mbps

    11.8Mbps

    SSL

    TCP Tx

    8.8Mbps

    8.5Mbps

    TCP Rx

    9.8Mbps

    9.8 Mbps