This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
详细的资料参考CC32xx Out of Box Application.pdf
CC32xx Out of Box Application
Overview
This Application demonstrates Out of Box Experience with CC3200
Launch Pad. It highlights the following features
1. Easy Connection to CC3200 Launchpad
• Direct Connection to Launchpad by using CC3200 device in
Access Point Mode(Default)
• Connection using TI SmartConfig [1]Technology
2. Easy access to CC3200 Using Internal HTTP server and on-board webcontent
3. Attractive Demos
• Home Automation
• Appliance Control
• Security System
• Thermostat
For more information please refer CC32xx Quick Start Guide
Usage
• The CC3200 Launchpad comes with all the required content flashed to run the application
• Refer Quick Start Guide for detailed information
• In case user flashed other SDK applications and need to download the out of box content again, follow below
steps
• Open <cc3200-sdk>\examples\out_of_box\html\out_of_box.ucf session file in Uniflash.
• Flash the files to the device. Detailed instructions at Uniflash User Guide.
• Run the reference application
1. Run From IDE (IAR/CCS)
• Open the Example Project as mentioned in the <cc3200-sdk>\docs\CC3200-Getting Started Guide.pdf
• Build and download the application to the board
2. Run From Flashed Binary
• Connect to CC3200 device as mentioned in Quick Start Guide, You will see below main page on your browser
Note: : In case device is coming up as AP (Jumper on VCC+P58) check Terminal prints to get to know device's AP
name.
注意CC3200的Out of Box 存在两种模式,第一种模式时AP模式此时Launchpad的 AP (Jumper on VCC+P58)模式,也就是需要Pin58脚通过跳线帽的方式连接到VCC中,如果拔掉这个跳线帽,则CC3200启动为Station模式。