那位前辈有64位的win10系统的ccs6.0开发平台,我是新手,电脑是64位的win10系统,想学习cc3200的芯片,但是没有开发平台,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
那位前辈有64位的win10系统的ccs6.0开发平台,我是新手,电脑是64位的win10系统,想学习cc3200的芯片,但是没有开发平台,谢谢
如下link下载,想要什么版本自己挑
http://processors.wiki.ti.com/index.php/Download_CCS
It is highly recommended to use the latest version of Code Composer Studio as patches are not provided for older versions.
There are two types of installers:
If you have an issue with the web installer not being able to connect to the internet then please try the off-line installer. If you need to update a computer that does not have internet access then download the offline installer and then transfer it to the computer without access and use the offline installer to update your installation.
Release | Build # | Date | Download | Notes |
6.2.0 | 6.2.0.00050 | Sept 14, 2016 | Web Installers: Windows Linux - 64-bit only MacOS |
|
6.2.0 | 6.2.0.00048 | Aug 31, 2016 | Web Installers: Windows Linux - 64-bit only MacOS |
|
6.1.3 | 6.1.3.00034 | Jul 2, 2016 | Web Installers: Windows Linux |
|
6.1.3 | 6.1.3.00033 | Apr 22, 2016 | Web Installers: Windows Linux |
|
6.1.2 | 6.1.2.00015 | Dec 23, 2015 | Web Installers: Windows Linux |
|
6.1.1 | 6.1.1.00022 | Sept 16, 2015 | Web Installers: Windows Linux |
|
6.1.0 | 6.1.0.00104 | Feb 25, 2015 | Web Installers: Windows Linux |
|
6.0.1 | 6.0.1.00040 | Aug 3, 2014 | Web Installers: Windows Linux |
|
6.0.1 | 6.0.1.00039 | July 22, 2014 | Web Installers: Windows Linux |
|
6.0.0 | 6.0.0.00190 | April 21, 2014 | Web Installers: Windows Linux |
|