那位前辈有64位的win10系统的ccs6.0开发平台,我是新手,电脑是64位的win10系统,想学习cc3200的芯片,但是没有开发平台,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
那位前辈有64位的win10系统的ccs6.0开发平台,我是新手,电脑是64位的win10系统,想学习cc3200的芯片,但是没有开发平台,谢谢
如下link下载,想要什么版本自己挑
http://processors.wiki.ti.com/index.php/Download_CCS
It is highly recommended to use the latest version of Code Composer Studio as patches are not provided for older versions.
There are two types of installers:
If you have an issue with the web installer not being able to connect to the internet then please try the off-line installer. If you need to update a computer that does not have internet access then download the offline installer and then transfer it to the computer without access and use the offline installer to update your installation.
| Release | Build # | Date | Download | Notes |
| 6.2.0 | 6.2.0.00050 | Sept 14, 2016 | Web Installers: Windows Linux - 64-bit only MacOS |
|
| 6.2.0 | 6.2.0.00048 | Aug 31, 2016 | Web Installers: Windows Linux - 64-bit only MacOS |
|
| 6.1.3 | 6.1.3.00034 | Jul 2, 2016 | Web Installers: Windows Linux |
|
| 6.1.3 | 6.1.3.00033 | Apr 22, 2016 | Web Installers: Windows Linux |
|
| 6.1.2 | 6.1.2.00015 | Dec 23, 2015 | Web Installers: Windows Linux |
|
| 6.1.1 | 6.1.1.00022 | Sept 16, 2015 | Web Installers: Windows Linux |
|
| 6.1.0 | 6.1.0.00104 | Feb 25, 2015 | Web Installers: Windows Linux |
|
| 6.0.1 | 6.0.1.00040 | Aug 3, 2014 | Web Installers: Windows Linux |
|
| 6.0.1 | 6.0.1.00039 | July 22, 2014 | Web Installers: Windows Linux |
|
| 6.0.0 | 6.0.0.00190 | April 21, 2014 | Web Installers: Windows Linux |
|