这是电路原理图,L4右端接CC3220芯片的38脚的波形出现了问题,与开发板不一样,其中CC3220的38管脚定义是Analog DC-DC switching node
下图是我板子上测试L4右端的波形图
局部放大后的图为
下图是开发板上L4右端测试的波形
它这个波形比较规律,为啥我板子上L4的波形就和开发板上的波形不一样啊??怎么回事啊??请帮我分析一下啊。谢谢了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这是电路原理图,L4右端接CC3220芯片的38脚的波形出现了问题,与开发板不一样,其中CC3220的38管脚定义是Analog DC-DC switching node
下图是我板子上测试L4右端的波形图
局部放大后的图为
下图是开发板上L4右端测试的波形
它这个波形比较规律,为啥我板子上L4的波形就和开发板上的波形不一样啊??怎么回事啊??请帮我分析一下啊。谢谢了
图中开发板波形周期是600ns左右,大概1.67MHz吧。我就是就是按照开发板原理图来的,参数也是对照手册的,布线基本上也是参照开发板来的,不知道为啥电感部分的波形不一致,是不是电感有问题啊??
Adams,
这些信号和DCDC的模式相关的,也就是说,和芯片的工作模式相关。
你测试的时候芯片在同样的模式下吗?
这个电压输出1.8V(电感左面)就对了。
BR.AZ