This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

咨询一下TI的wifi方案CC32xx系列和乐鑫的esp32相比有什么优势?

Other Parts Discussed in Thread: CC3200

目前对比一下,似乎esp32性价比更高,也支持freeRTOS,目测好像TI的零售价至少是乐鑫的3倍不止,不知TI的优势在什么地方?

1、esp32 512KB RAM,CC32xx只有一半256KB RAM

2、esp32最高主频能到240Mhz,性能非常强大,CC32xx好像只有80Mhz,反正wifi又不缺电,又不是电池供电,功耗低不低无所谓不是

3、另外esp32还内置BLE,TI根本不支持,另外需要加IC,都是成本

  • 这个,单从参数上ESP32肯定是更好。esp8266这种作为WIFI收发器也是超高性价比。
    而CC3200是作为单片机推出的。TI的性能上更加稳定可靠。TI的产品一向都是比较贵一点。但是性能上更加稳定可靠。就跟工业交换机和家庭交换机的区别一样。
  • 我觉得单是说从单片机角度说,TI几乎没有性价比可言,我们都知道,乐鑫虽然核心部分代码不开放,但是提供了SDK,系统大量的资源完全可以提供给二次开发,单片机能完成的事情,esp32好像全部都能完成,另外esp32工作温度范围也能达到 –40°C 到 +125°C,工业温度好像也是如此了

    另外,小米之前宣布9.9元的wifi模块可以全线接入宜家的灯泡,其实用也是众所周知的esp8266系列,wifi iot领域好像目前没有哪家能做过乐鑫的,反正功耗在wifi来讲算不了什么,都是AC供电

  • 用CC32就不要讨论性价比了。各有各的特色,我做廉价产品也用8266,几块钱成本。跑nodeMCU固件,一片就搞定。
    用CC32xx的有自己的优点。就跟51单片机一样,好多厂家做,价格不同,有好多便宜的参数更给力,但是还是有人选择配置低,价格贵的国外品牌。
  • 不是性价比,有时候是情怀
  • 我认为是这样的

    1.产品的生产问题,TI的生产工艺,技术,做出来的产品的性能很可能是最好的。单纯从数据手册来看,是看不出什么问题的,就像有些国产ADC一样,从价格和手册的性能来看,和TI的ADC差不多,可是实际效果差的多了,尤其是极端的环境下。当然,消费电子领域,TI的价格是干不过乐鑫的,工业的领域,不在乎这点成本,肯定会选择TI的芯片的。

    2.产品的定价问题,TI的产品在前,乐鑫的产品在后,他的定价肯定要低于TI的,不然凭什么竞争呀,再加上其他成本,价格肯定是低廉的。

    3.我觉得TI产品的优势在于生态链,随便某一个行业,你很难不用TI的芯片,他的生态链可以使用他的芯片集成在一起。就好像小米的生态链一样,还有比小米更性价比高的产品,为什么不用呢,因为他的生态链已经做得很好了。