This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS或IAR 连接CC3200 launchpad debug失败,提示无法连接

Other Parts Discussed in Thread: CC3200

最近刚刚拿到一块CC3200 launch pad,按照《CC3200-Getting_Started_Guide》文档中的介绍操作,但无论是ccs还是IAR,在download and debug时都失败,提示无法连接。但Tera Term显示串口连接正常。具体问题如下:

1. cc3200 lauch pad 版本:

NWP Version: 2.2.0.001
MAC Version: 31.1.2.0.2
PHY Version: 1.0.3.17
HW Version: 0x4000010

2. TI SDK版本为 1.3.0

3. CCS版本为6.1.1.00022,按《CC3200-Getting_Started_Guide》操作到debug步骤时,弹出消息框,提示错误信息如下:

Error connecting to the target

4. IAR版本为 8.30.1,按CC3200-Getting_Started_Guide》操作到download and debug时,弹出消息框,提示错误信息如下:

Fatal error:**ERROR**:Unable to connect - Check hardware,speed and interface selected Session aborted!

5. 使用Tera term监控串口,发现从PC上拔掉连接lauch pad的Micro usb线时 tera term显示【未连接】,插上USB线则【未连接】字样消失,串口号(电脑设备管理中看到的是COM6)和波特率(115200)都检查过,没有发现问题

本人小白,向各位大侠求教,这可能是什么原因导致的?

谢谢!