This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【CC3200 评测】CC3200-LAUNCHXL开发板初体验

Other Parts Discussed in Thread: CC3200-LAUNCHXL

  • 开箱介绍

收到的

  1. .CC3200-LAUNCHXL开发板一块
  2.  USB线一根
  3. 跳线帽一个

  • 初上手体验

 使用板子默认的跳线(如下 图),然后接入电源。LED灯的D5和D6长亮,D7熄灭,说明进入了AP模式。

可以用手机或笔记本连接上mysimplelink-112D82。如图

笔记本最大连接距离大概10M,手机只有8M不到。

在游览器里输入http://MySimpleLink.net可以打开demo页面,参照http://www.ti.com/CC3200launchpadstart 可以进行简单的demo测试

 DEMO

预设了四个简单的demo,包括控制草坪洒水器,洗衣机,室内温度传感和门锁控制。

SETUP

板子的设置页面,主要设置密码和wifi名字之类的简单设置。